flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxProperty Class Referenceabstract

#include <flxCoreProps.h>

Inheritance diagram for flxProperty:
flxDescriptor _flxPropertyBase< T, false, false > _flxPropertyBase< _flxClock, false, false > _flxPropertyBase< flxDevACS37800, false, false > _flxPropertyBase< flxDevADS1015, false, false > _flxPropertyBase< flxDevADS122C04, false, false > _flxPropertyBase< flxDevAMG8833, false, false > _flxPropertyBase< flxDevAS7265X, false, false > _flxPropertyBase< flxDevAS7331, false, false > _flxPropertyBase< flxDevAS7343, false, false > _flxPropertyBase< flxDevAnalogPin, false, false > _flxPropertyBase< flxDevBMP581, false, false > _flxPropertyBase< flxDevBMV080, false, false > _flxPropertyBase< flxDevButton, false, false > _flxPropertyBase< flxDevENS160, false, false > _flxPropertyBase< flxDevFS3000, false, false > _flxPropertyBase< flxDevGNSS, false, false > _flxPropertyBase< flxDevISM330Base, false, false > _flxPropertyBase< flxDevMCP9600, false, false > _flxPropertyBase< flxDevMMC5983Base, false, false > _flxPropertyBase< flxDevNAU7802, false, false > _flxPropertyBase< flxDevOPT4048, false, false > _flxPropertyBase< flxDevPASCO2V01, false, false > _flxPropertyBase< flxDevSCD30, false, false > _flxPropertyBase< flxDevSCD40, false, false > _flxPropertyBase< flxDevSDP3X, false, false > _flxPropertyBase< flxDevSEN54, false, false > _flxPropertyBase< flxDevSTC31, false, false > _flxPropertyBase< flxDevSTHS34PF80, false, false > _flxPropertyBase< flxDevSerial, false, false > _flxPropertyBase< flxDevSoilMoisture, false, false > _flxPropertyBase< flxDevTMF882X, false, false > _flxPropertyBase< flxDevTwist, false, false > _flxPropertyBase< flxDevVCNL4040, false, false > _flxPropertyBase< flxDevVEML6075, false, false > _flxPropertyBase< flxDevVEML7700, false, false > _flxPropertyBase< flxDevVL53L1X, false, false > _flxPropertyBase< flxDevVL53L5, false, false > _flxPropertyBase< flxFileRotate, false, false > _flxPropertyBase< flxIoTArduino, false, false > _flxPropertyBase< flxLogger, false, false > _flxPropertyBase< flxOptEnableDevice, false, false > _flxPropertyBase< flxOptExtSerial, false, false > _flxPropertyBase< flxOptInterruptEvent, false, false > _flxPropertyBase< flxSettingsSave, false, false > _flxPropertyBase< flxTimer, false, false > _flxPropertyBaseString< false, false > _flxPropertyBase< T, HIDDEN, SECURE > _flxPropertyBaseString< HIDDEN, SECURE >

Public Member Functions

virtual flxDataType_t type (void)=0
 
virtual flxEditResult_t editValue (flxDataEditor &)=0
 
virtual flxDataLimit * dataLimit (void)=0
 
virtual bool setValue (flxDataVariable &)=0
 
virtual flxDataVariable getValue (void)=0
 
virtual bool hidden (void)=0
 
virtual void setHidden (void)=0
 
virtual bool secure (void)=0
 
virtual size_t size (void)
 
virtual size_t save_size (void)
 
virtual std::string to_string ()
 
virtual bool save (flxStorageBlock *)=0
 
virtual bool restore (flxStorageBlock *)=0
 
- Public Member Functions inherited from flxDescriptor
 flxDescriptor ()
 
void setName (const char *new_name)
 Set the Name object - storing the pointer to the provided string No allocation is performed. If the previous name was allocated, it is freed. More...
 
void setName (const char *new_name, const char *new_desc)
 Set the Name object and the Description for the object. Both strings are constants. More...
 
void setName (char *new_name)
 Set the Name object, but makes a copy of the input string since the input is not const. If the previous name was allocated, it is freed. More...
 
const char * name ()
 Return a const char pointer to the name of the object. More...
 
std::string name_ (void)
 Returns a std::string of the name of the object. More...
 
void setDescription (const char *new_desc)
 Set the Description object - the input value is constant and not copied. If the previous description was allocated, it is freed. More...
 
void setDescription (char *new_desc)
 Set the Description object - the input value is not constant and is copied. If the previous description was allocated, it is freed. More...
 
const char * description ()
 Return the constant C string pointer to the description of the object. More...
 
std::string description_ (void)
 Return the description of the object as a std::string. More...
 
void setTitle (const char *title)
 Set the Title object - the title is optional and is used mostly for UX or organizational purposes. The input value is constant and not copied. If the previous title was allocated, it is freed. More...
 
void setTitleAlloc (char *new_title)
 Set the Title of the object , but make an explict copy of the provided string. More...
 
const char * title (void)
 Return the C constant string pointer to the title of the object. More...
 

Additional Inherited Members

- Protected Attributes inherited from flxDescriptor
const char * _name
 
bool _nameAlloc
 
const char * _desc
 
bool _descAlloc
 
const char * _title
 
bool _titleAlloc
 

Member Function Documentation

◆ dataLimit()

virtual flxDataLimit * flxProperty::dataLimit ( void  )
pure virtual

Implemented in _flxPropertyBase< T, HIDDEN, SECURE >, _flxPropertyBase< T, false, false >, _flxPropertyBase< _flxClock, false, false >, _flxPropertyBase< flxDevACS37800, false, false >, _flxPropertyBase< flxDevADS1015, false, false >, _flxPropertyBase< flxDevADS122C04, false, false >, _flxPropertyBase< flxDevAMG8833, false, false >, _flxPropertyBase< flxDevAS7265X, false, false >, _flxPropertyBase< flxDevAS7331, false, false >, _flxPropertyBase< flxDevAS7343, false, false >, _flxPropertyBase< flxDevAnalogPin, false, false >, _flxPropertyBase< flxDevBMP581, false, false >, _flxPropertyBase< flxDevBMV080, false, false >, _flxPropertyBase< flxDevButton, false, false >, _flxPropertyBase< flxDevENS160, false, false >, _flxPropertyBase< flxDevFS3000, false, false >, _flxPropertyBase< flxDevGNSS, false, false >, _flxPropertyBase< flxDevISM330Base, false, false >, _flxPropertyBase< flxDevMCP9600, false, false >, _flxPropertyBase< flxDevMMC5983Base, false, false >, _flxPropertyBase< flxDevNAU7802, false, false >, _flxPropertyBase< flxDevOPT4048, false, false >, _flxPropertyBase< flxDevPASCO2V01, false, false >, _flxPropertyBase< flxDevSCD30, false, false >, _flxPropertyBase< flxDevSCD40, false, false >, _flxPropertyBase< flxDevSDP3X, false, false >, _flxPropertyBase< flxDevSEN54, false, false >, _flxPropertyBase< flxDevSTC31, false, false >, _flxPropertyBase< flxDevSTHS34PF80, false, false >, _flxPropertyBase< flxDevSerial, false, false >, _flxPropertyBase< flxDevSoilMoisture, false, false >, _flxPropertyBase< flxDevTMF882X, false, false >, _flxPropertyBase< flxDevTwist, false, false >, _flxPropertyBase< flxDevVCNL4040, false, false >, _flxPropertyBase< flxDevVEML6075, false, false >, _flxPropertyBase< flxDevVEML7700, false, false >, _flxPropertyBase< flxDevVL53L1X, false, false >, _flxPropertyBase< flxDevVL53L5, false, false >, _flxPropertyBase< flxFileRotate, false, false >, _flxPropertyBase< flxIoTArduino, false, false >, _flxPropertyBase< flxLogger, false, false >, _flxPropertyBase< flxOptEnableDevice, false, false >, _flxPropertyBase< flxOptExtSerial, false, false >, _flxPropertyBase< flxOptInterruptEvent, false, false >, _flxPropertyBase< flxSettingsSave, false, false >, _flxPropertyBase< flxTimer, false, false >, _flxPropertyBaseString< HIDDEN, SECURE >, and _flxPropertyBaseString< false, false >.

◆ editValue()

virtual flxEditResult_t flxProperty::editValue ( flxDataEditor &  )
pure virtual

Implemented in _flxPropertyBase< T, HIDDEN, SECURE >, _flxPropertyBase< T, false, false >, _flxPropertyBase< _flxClock, false, false >, _flxPropertyBase< flxDevACS37800, false, false >, _flxPropertyBase< flxDevADS1015, false, false >, _flxPropertyBase< flxDevADS122C04, false, false >, _flxPropertyBase< flxDevAMG8833, false, false >, _flxPropertyBase< flxDevAS7265X, false, false >, _flxPropertyBase< flxDevAS7331, false, false >, _flxPropertyBase< flxDevAS7343, false, false >, _flxPropertyBase< flxDevAnalogPin, false, false >, _flxPropertyBase< flxDevBMP581, false, false >, _flxPropertyBase< flxDevBMV080, false, false >, _flxPropertyBase< flxDevButton, false, false >, _flxPropertyBase< flxDevENS160, false, false >, _flxPropertyBase< flxDevFS3000, false, false >, _flxPropertyBase< flxDevGNSS, false, false >, _flxPropertyBase< flxDevISM330Base, false, false >, _flxPropertyBase< flxDevMCP9600, false, false >, _flxPropertyBase< flxDevMMC5983Base, false, false >, _flxPropertyBase< flxDevNAU7802, false, false >, _flxPropertyBase< flxDevOPT4048, false, false >, _flxPropertyBase< flxDevPASCO2V01, false, false >, _flxPropertyBase< flxDevSCD30, false, false >, _flxPropertyBase< flxDevSCD40, false, false >, _flxPropertyBase< flxDevSDP3X, false, false >, _flxPropertyBase< flxDevSEN54, false, false >, _flxPropertyBase< flxDevSTC31, false, false >, _flxPropertyBase< flxDevSTHS34PF80, false, false >, _flxPropertyBase< flxDevSerial, false, false >, _flxPropertyBase< flxDevSoilMoisture, false, false >, _flxPropertyBase< flxDevTMF882X, false, false >, _flxPropertyBase< flxDevTwist, false, false >, _flxPropertyBase< flxDevVCNL4040, false, false >, _flxPropertyBase< flxDevVEML6075, false, false >, _flxPropertyBase< flxDevVEML7700, false, false >, _flxPropertyBase< flxDevVL53L1X, false, false >, _flxPropertyBase< flxDevVL53L5, false, false >, _flxPropertyBase< flxFileRotate, false, false >, _flxPropertyBase< flxIoTArduino, false, false >, _flxPropertyBase< flxLogger, false, false >, _flxPropertyBase< flxOptEnableDevice, false, false >, _flxPropertyBase< flxOptExtSerial, false, false >, _flxPropertyBase< flxOptInterruptEvent, false, false >, _flxPropertyBase< flxSettingsSave, false, false >, _flxPropertyBase< flxTimer, false, false >, _flxPropertyBaseString< HIDDEN, SECURE >, and _flxPropertyBaseString< false, false >.

◆ getValue()

virtual flxDataVariable flxProperty::getValue ( void  )
pure virtual

Implemented in _flxPropertyBase< T, HIDDEN, SECURE >, _flxPropertyBase< T, false, false >, _flxPropertyBase< _flxClock, false, false >, _flxPropertyBase< flxDevACS37800, false, false >, _flxPropertyBase< flxDevADS1015, false, false >, _flxPropertyBase< flxDevADS122C04, false, false >, _flxPropertyBase< flxDevAMG8833, false, false >, _flxPropertyBase< flxDevAS7265X, false, false >, _flxPropertyBase< flxDevAS7331, false, false >, _flxPropertyBase< flxDevAS7343, false, false >, _flxPropertyBase< flxDevAnalogPin, false, false >, _flxPropertyBase< flxDevBMP581, false, false >, _flxPropertyBase< flxDevBMV080, false, false >, _flxPropertyBase< flxDevButton, false, false >, _flxPropertyBase< flxDevENS160, false, false >, _flxPropertyBase< flxDevFS3000, false, false >, _flxPropertyBase< flxDevGNSS, false, false >, _flxPropertyBase< flxDevISM330Base, false, false >, _flxPropertyBase< flxDevMCP9600, false, false >, _flxPropertyBase< flxDevMMC5983Base, false, false >, _flxPropertyBase< flxDevNAU7802, false, false >, _flxPropertyBase< flxDevOPT4048, false, false >, _flxPropertyBase< flxDevPASCO2V01, false, false >, _flxPropertyBase< flxDevSCD30, false, false >, _flxPropertyBase< flxDevSCD40, false, false >, _flxPropertyBase< flxDevSDP3X, false, false >, _flxPropertyBase< flxDevSEN54, false, false >, _flxPropertyBase< flxDevSTC31, false, false >, _flxPropertyBase< flxDevSTHS34PF80, false, false >, _flxPropertyBase< flxDevSerial, false, false >, _flxPropertyBase< flxDevSoilMoisture, false, false >, _flxPropertyBase< flxDevTMF882X, false, false >, _flxPropertyBase< flxDevTwist, false, false >, _flxPropertyBase< flxDevVCNL4040, false, false >, _flxPropertyBase< flxDevVEML6075, false, false >, _flxPropertyBase< flxDevVEML7700, false, false >, _flxPropertyBase< flxDevVL53L1X, false, false >, _flxPropertyBase< flxDevVL53L5, false, false >, _flxPropertyBase< flxFileRotate, false, false >, _flxPropertyBase< flxIoTArduino, false, false >, _flxPropertyBase< flxLogger, false, false >, _flxPropertyBase< flxOptEnableDevice, false, false >, _flxPropertyBase< flxOptExtSerial, false, false >, _flxPropertyBase< flxOptInterruptEvent, false, false >, _flxPropertyBase< flxSettingsSave, false, false >, _flxPropertyBase< flxTimer, false, false >, _flxPropertyBaseString< HIDDEN, SECURE >, and _flxPropertyBaseString< false, false >.

◆ hidden()

virtual bool flxProperty::hidden ( void  )
pure virtual

Implemented in _flxPropertyBase< T, HIDDEN, SECURE >, _flxPropertyBase< T, false, false >, _flxPropertyBase< _flxClock, false, false >, _flxPropertyBase< flxDevACS37800, false, false >, _flxPropertyBase< flxDevADS1015, false, false >, _flxPropertyBase< flxDevADS122C04, false, false >, _flxPropertyBase< flxDevAMG8833, false, false >, _flxPropertyBase< flxDevAS7265X, false, false >, _flxPropertyBase< flxDevAS7331, false, false >, _flxPropertyBase< flxDevAS7343, false, false >, _flxPropertyBase< flxDevAnalogPin, false, false >, _flxPropertyBase< flxDevBMP581, false, false >, _flxPropertyBase< flxDevBMV080, false, false >, _flxPropertyBase< flxDevButton, false, false >, _flxPropertyBase< flxDevENS160, false, false >, _flxPropertyBase< flxDevFS3000, false, false >, _flxPropertyBase< flxDevGNSS, false, false >, _flxPropertyBase< flxDevISM330Base, false, false >, _flxPropertyBase< flxDevMCP9600, false, false >, _flxPropertyBase< flxDevMMC5983Base, false, false >, _flxPropertyBase< flxDevNAU7802, false, false >, _flxPropertyBase< flxDevOPT4048, false, false >, _flxPropertyBase< flxDevPASCO2V01, false, false >, _flxPropertyBase< flxDevSCD30, false, false >, _flxPropertyBase< flxDevSCD40, false, false >, _flxPropertyBase< flxDevSDP3X, false, false >, _flxPropertyBase< flxDevSEN54, false, false >, _flxPropertyBase< flxDevSTC31, false, false >, _flxPropertyBase< flxDevSTHS34PF80, false, false >, _flxPropertyBase< flxDevSerial, false, false >, _flxPropertyBase< flxDevSoilMoisture, false, false >, _flxPropertyBase< flxDevTMF882X, false, false >, _flxPropertyBase< flxDevTwist, false, false >, _flxPropertyBase< flxDevVCNL4040, false, false >, _flxPropertyBase< flxDevVEML6075, false, false >, _flxPropertyBase< flxDevVEML7700, false, false >, _flxPropertyBase< flxDevVL53L1X, false, false >, _flxPropertyBase< flxDevVL53L5, false, false >, _flxPropertyBase< flxFileRotate, false, false >, _flxPropertyBase< flxIoTArduino, false, false >, _flxPropertyBase< flxLogger, false, false >, _flxPropertyBase< flxOptEnableDevice, false, false >, _flxPropertyBase< flxOptExtSerial, false, false >, _flxPropertyBase< flxOptInterruptEvent, false, false >, _flxPropertyBase< flxSettingsSave, false, false >, _flxPropertyBase< flxTimer, false, false >, _flxPropertyBaseString< HIDDEN, SECURE >, and _flxPropertyBaseString< false, false >.

◆ restore()

virtual bool flxProperty::restore ( flxStorageBlock *  )
pure virtual

Implemented in _flxPropertyBase< T, HIDDEN, SECURE >, _flxPropertyBase< T, false, false >, _flxPropertyBase< _flxClock, false, false >, _flxPropertyBase< flxDevACS37800, false, false >, _flxPropertyBase< flxDevADS1015, false, false >, _flxPropertyBase< flxDevADS122C04, false, false >, _flxPropertyBase< flxDevAMG8833, false, false >, _flxPropertyBase< flxDevAS7265X, false, false >, _flxPropertyBase< flxDevAS7331, false, false >, _flxPropertyBase< flxDevAS7343, false, false >, _flxPropertyBase< flxDevAnalogPin, false, false >, _flxPropertyBase< flxDevBMP581, false, false >, _flxPropertyBase< flxDevBMV080, false, false >, _flxPropertyBase< flxDevButton, false, false >, _flxPropertyBase< flxDevENS160, false, false >, _flxPropertyBase< flxDevFS3000, false, false >, _flxPropertyBase< flxDevGNSS, false, false >, _flxPropertyBase< flxDevISM330Base, false, false >, _flxPropertyBase< flxDevMCP9600, false, false >, _flxPropertyBase< flxDevMMC5983Base, false, false >, _flxPropertyBase< flxDevNAU7802, false, false >, _flxPropertyBase< flxDevOPT4048, false, false >, _flxPropertyBase< flxDevPASCO2V01, false, false >, _flxPropertyBase< flxDevSCD30, false, false >, _flxPropertyBase< flxDevSCD40, false, false >, _flxPropertyBase< flxDevSDP3X, false, false >, _flxPropertyBase< flxDevSEN54, false, false >, _flxPropertyBase< flxDevSTC31, false, false >, _flxPropertyBase< flxDevSTHS34PF80, false, false >, _flxPropertyBase< flxDevSerial, false, false >, _flxPropertyBase< flxDevSoilMoisture, false, false >, _flxPropertyBase< flxDevTMF882X, false, false >, _flxPropertyBase< flxDevTwist, false, false >, _flxPropertyBase< flxDevVCNL4040, false, false >, _flxPropertyBase< flxDevVEML6075, false, false >, _flxPropertyBase< flxDevVEML7700, false, false >, _flxPropertyBase< flxDevVL53L1X, false, false >, _flxPropertyBase< flxDevVL53L5, false, false >, _flxPropertyBase< flxFileRotate, false, false >, _flxPropertyBase< flxIoTArduino, false, false >, _flxPropertyBase< flxLogger, false, false >, _flxPropertyBase< flxOptEnableDevice, false, false >, _flxPropertyBase< flxOptExtSerial, false, false >, _flxPropertyBase< flxOptInterruptEvent, false, false >, _flxPropertyBase< flxSettingsSave, false, false >, _flxPropertyBase< flxTimer, false, false >, _flxPropertyBaseString< HIDDEN, SECURE >, and _flxPropertyBaseString< false, false >.

◆ save()

virtual bool flxProperty::save ( flxStorageBlock *  )
pure virtual

Implemented in _flxPropertyBase< T, HIDDEN, SECURE >, _flxPropertyBase< T, false, false >, _flxPropertyBase< _flxClock, false, false >, _flxPropertyBase< flxDevACS37800, false, false >, _flxPropertyBase< flxDevADS1015, false, false >, _flxPropertyBase< flxDevADS122C04, false, false >, _flxPropertyBase< flxDevAMG8833, false, false >, _flxPropertyBase< flxDevAS7265X, false, false >, _flxPropertyBase< flxDevAS7331, false, false >, _flxPropertyBase< flxDevAS7343, false, false >, _flxPropertyBase< flxDevAnalogPin, false, false >, _flxPropertyBase< flxDevBMP581, false, false >, _flxPropertyBase< flxDevBMV080, false, false >, _flxPropertyBase< flxDevButton, false, false >, _flxPropertyBase< flxDevENS160, false, false >, _flxPropertyBase< flxDevFS3000, false, false >, _flxPropertyBase< flxDevGNSS, false, false >, _flxPropertyBase< flxDevISM330Base, false, false >, _flxPropertyBase< flxDevMCP9600, false, false >, _flxPropertyBase< flxDevMMC5983Base, false, false >, _flxPropertyBase< flxDevNAU7802, false, false >, _flxPropertyBase< flxDevOPT4048, false, false >, _flxPropertyBase< flxDevPASCO2V01, false, false >, _flxPropertyBase< flxDevSCD30, false, false >, _flxPropertyBase< flxDevSCD40, false, false >, _flxPropertyBase< flxDevSDP3X, false, false >, _flxPropertyBase< flxDevSEN54, false, false >, _flxPropertyBase< flxDevSTC31, false, false >, _flxPropertyBase< flxDevSTHS34PF80, false, false >, _flxPropertyBase< flxDevSerial, false, false >, _flxPropertyBase< flxDevSoilMoisture, false, false >, _flxPropertyBase< flxDevTMF882X, false, false >, _flxPropertyBase< flxDevTwist, false, false >, _flxPropertyBase< flxDevVCNL4040, false, false >, _flxPropertyBase< flxDevVEML6075, false, false >, _flxPropertyBase< flxDevVEML7700, false, false >, _flxPropertyBase< flxDevVL53L1X, false, false >, _flxPropertyBase< flxDevVL53L5, false, false >, _flxPropertyBase< flxFileRotate, false, false >, _flxPropertyBase< flxIoTArduino, false, false >, _flxPropertyBase< flxLogger, false, false >, _flxPropertyBase< flxOptEnableDevice, false, false >, _flxPropertyBase< flxOptExtSerial, false, false >, _flxPropertyBase< flxOptInterruptEvent, false, false >, _flxPropertyBase< flxSettingsSave, false, false >, _flxPropertyBase< flxTimer, false, false >, _flxPropertyBaseString< HIDDEN, SECURE >, and _flxPropertyBaseString< false, false >.

◆ save_size()

virtual size_t flxProperty::save_size ( void  )
inlinevirtual

Reimplemented in _flxPropertyBase< T, HIDDEN, SECURE >, _flxPropertyBase< T, false, false >, _flxPropertyBase< _flxClock, false, false >, _flxPropertyBase< flxDevACS37800, false, false >, _flxPropertyBase< flxDevADS1015, false, false >, _flxPropertyBase< flxDevADS122C04, false, false >, _flxPropertyBase< flxDevAMG8833, false, false >, _flxPropertyBase< flxDevAS7265X, false, false >, _flxPropertyBase< flxDevAS7331, false, false >, _flxPropertyBase< flxDevAS7343, false, false >, _flxPropertyBase< flxDevAnalogPin, false, false >, _flxPropertyBase< flxDevBMP581, false, false >, _flxPropertyBase< flxDevBMV080, false, false >, _flxPropertyBase< flxDevButton, false, false >, _flxPropertyBase< flxDevENS160, false, false >, _flxPropertyBase< flxDevFS3000, false, false >, _flxPropertyBase< flxDevGNSS, false, false >, _flxPropertyBase< flxDevISM330Base, false, false >, _flxPropertyBase< flxDevMCP9600, false, false >, _flxPropertyBase< flxDevMMC5983Base, false, false >, _flxPropertyBase< flxDevNAU7802, false, false >, _flxPropertyBase< flxDevOPT4048, false, false >, _flxPropertyBase< flxDevPASCO2V01, false, false >, _flxPropertyBase< flxDevSCD30, false, false >, _flxPropertyBase< flxDevSCD40, false, false >, _flxPropertyBase< flxDevSDP3X, false, false >, _flxPropertyBase< flxDevSEN54, false, false >, _flxPropertyBase< flxDevSTC31, false, false >, _flxPropertyBase< flxDevSTHS34PF80, false, false >, _flxPropertyBase< flxDevSerial, false, false >, _flxPropertyBase< flxDevSoilMoisture, false, false >, _flxPropertyBase< flxDevTMF882X, false, false >, _flxPropertyBase< flxDevTwist, false, false >, _flxPropertyBase< flxDevVCNL4040, false, false >, _flxPropertyBase< flxDevVEML6075, false, false >, _flxPropertyBase< flxDevVEML7700, false, false >, _flxPropertyBase< flxDevVL53L1X, false, false >, _flxPropertyBase< flxDevVL53L5, false, false >, _flxPropertyBase< flxFileRotate, false, false >, _flxPropertyBase< flxIoTArduino, false, false >, _flxPropertyBase< flxLogger, false, false >, _flxPropertyBase< flxOptEnableDevice, false, false >, _flxPropertyBase< flxOptExtSerial, false, false >, _flxPropertyBase< flxOptInterruptEvent, false, false >, _flxPropertyBase< flxSettingsSave, false, false >, _flxPropertyBase< flxTimer, false, false >, _flxPropertyBaseString< HIDDEN, SECURE >, and _flxPropertyBaseString< false, false >.

◆ secure()

virtual bool flxProperty::secure ( void  )
pure virtual

Implemented in _flxPropertyBase< T, HIDDEN, SECURE >, _flxPropertyBase< T, false, false >, _flxPropertyBase< _flxClock, false, false >, _flxPropertyBase< flxDevACS37800, false, false >, _flxPropertyBase< flxDevADS1015, false, false >, _flxPropertyBase< flxDevADS122C04, false, false >, _flxPropertyBase< flxDevAMG8833, false, false >, _flxPropertyBase< flxDevAS7265X, false, false >, _flxPropertyBase< flxDevAS7331, false, false >, _flxPropertyBase< flxDevAS7343, false, false >, _flxPropertyBase< flxDevAnalogPin, false, false >, _flxPropertyBase< flxDevBMP581, false, false >, _flxPropertyBase< flxDevBMV080, false, false >, _flxPropertyBase< flxDevButton, false, false >, _flxPropertyBase< flxDevENS160, false, false >, _flxPropertyBase< flxDevFS3000, false, false >, _flxPropertyBase< flxDevGNSS, false, false >, _flxPropertyBase< flxDevISM330Base, false, false >, _flxPropertyBase< flxDevMCP9600, false, false >, _flxPropertyBase< flxDevMMC5983Base, false, false >, _flxPropertyBase< flxDevNAU7802, false, false >, _flxPropertyBase< flxDevOPT4048, false, false >, _flxPropertyBase< flxDevPASCO2V01, false, false >, _flxPropertyBase< flxDevSCD30, false, false >, _flxPropertyBase< flxDevSCD40, false, false >, _flxPropertyBase< flxDevSDP3X, false, false >, _flxPropertyBase< flxDevSEN54, false, false >, _flxPropertyBase< flxDevSTC31, false, false >, _flxPropertyBase< flxDevSTHS34PF80, false, false >, _flxPropertyBase< flxDevSerial, false, false >, _flxPropertyBase< flxDevSoilMoisture, false, false >, _flxPropertyBase< flxDevTMF882X, false, false >, _flxPropertyBase< flxDevTwist, false, false >, _flxPropertyBase< flxDevVCNL4040, false, false >, _flxPropertyBase< flxDevVEML6075, false, false >, _flxPropertyBase< flxDevVEML7700, false, false >, _flxPropertyBase< flxDevVL53L1X, false, false >, _flxPropertyBase< flxDevVL53L5, false, false >, _flxPropertyBase< flxFileRotate, false, false >, _flxPropertyBase< flxIoTArduino, false, false >, _flxPropertyBase< flxLogger, false, false >, _flxPropertyBase< flxOptEnableDevice, false, false >, _flxPropertyBase< flxOptExtSerial, false, false >, _flxPropertyBase< flxOptInterruptEvent, false, false >, _flxPropertyBase< flxSettingsSave, false, false >, _flxPropertyBase< flxTimer, false, false >, _flxPropertyBaseString< HIDDEN, SECURE >, and _flxPropertyBaseString< false, false >.

◆ setHidden()

virtual void flxProperty::setHidden ( void  )
pure virtual

Implemented in _flxPropertyBase< T, HIDDEN, SECURE >, _flxPropertyBase< T, false, false >, _flxPropertyBase< _flxClock, false, false >, _flxPropertyBase< flxDevACS37800, false, false >, _flxPropertyBase< flxDevADS1015, false, false >, _flxPropertyBase< flxDevADS122C04, false, false >, _flxPropertyBase< flxDevAMG8833, false, false >, _flxPropertyBase< flxDevAS7265X, false, false >, _flxPropertyBase< flxDevAS7331, false, false >, _flxPropertyBase< flxDevAS7343, false, false >, _flxPropertyBase< flxDevAnalogPin, false, false >, _flxPropertyBase< flxDevBMP581, false, false >, _flxPropertyBase< flxDevBMV080, false, false >, _flxPropertyBase< flxDevButton, false, false >, _flxPropertyBase< flxDevENS160, false, false >, _flxPropertyBase< flxDevFS3000, false, false >, _flxPropertyBase< flxDevGNSS, false, false >, _flxPropertyBase< flxDevISM330Base, false, false >, _flxPropertyBase< flxDevMCP9600, false, false >, _flxPropertyBase< flxDevMMC5983Base, false, false >, _flxPropertyBase< flxDevNAU7802, false, false >, _flxPropertyBase< flxDevOPT4048, false, false >, _flxPropertyBase< flxDevPASCO2V01, false, false >, _flxPropertyBase< flxDevSCD30, false, false >, _flxPropertyBase< flxDevSCD40, false, false >, _flxPropertyBase< flxDevSDP3X, false, false >, _flxPropertyBase< flxDevSEN54, false, false >, _flxPropertyBase< flxDevSTC31, false, false >, _flxPropertyBase< flxDevSTHS34PF80, false, false >, _flxPropertyBase< flxDevSerial, false, false >, _flxPropertyBase< flxDevSoilMoisture, false, false >, _flxPropertyBase< flxDevTMF882X, false, false >, _flxPropertyBase< flxDevTwist, false, false >, _flxPropertyBase< flxDevVCNL4040, false, false >, _flxPropertyBase< flxDevVEML6075, false, false >, _flxPropertyBase< flxDevVEML7700, false, false >, _flxPropertyBase< flxDevVL53L1X, false, false >, _flxPropertyBase< flxDevVL53L5, false, false >, _flxPropertyBase< flxFileRotate, false, false >, _flxPropertyBase< flxIoTArduino, false, false >, _flxPropertyBase< flxLogger, false, false >, _flxPropertyBase< flxOptEnableDevice, false, false >, _flxPropertyBase< flxOptExtSerial, false, false >, _flxPropertyBase< flxOptInterruptEvent, false, false >, _flxPropertyBase< flxSettingsSave, false, false >, _flxPropertyBase< flxTimer, false, false >, _flxPropertyBaseString< HIDDEN, SECURE >, and _flxPropertyBaseString< false, false >.

◆ setValue()

virtual bool flxProperty::setValue ( flxDataVariable &  )
pure virtual

Implemented in _flxPropertyBase< T, HIDDEN, SECURE >, _flxPropertyBase< T, false, false >, _flxPropertyBase< _flxClock, false, false >, _flxPropertyBase< flxDevACS37800, false, false >, _flxPropertyBase< flxDevADS1015, false, false >, _flxPropertyBase< flxDevADS122C04, false, false >, _flxPropertyBase< flxDevAMG8833, false, false >, _flxPropertyBase< flxDevAS7265X, false, false >, _flxPropertyBase< flxDevAS7331, false, false >, _flxPropertyBase< flxDevAS7343, false, false >, _flxPropertyBase< flxDevAnalogPin, false, false >, _flxPropertyBase< flxDevBMP581, false, false >, _flxPropertyBase< flxDevBMV080, false, false >, _flxPropertyBase< flxDevButton, false, false >, _flxPropertyBase< flxDevENS160, false, false >, _flxPropertyBase< flxDevFS3000, false, false >, _flxPropertyBase< flxDevGNSS, false, false >, _flxPropertyBase< flxDevISM330Base, false, false >, _flxPropertyBase< flxDevMCP9600, false, false >, _flxPropertyBase< flxDevMMC5983Base, false, false >, _flxPropertyBase< flxDevNAU7802, false, false >, _flxPropertyBase< flxDevOPT4048, false, false >, _flxPropertyBase< flxDevPASCO2V01, false, false >, _flxPropertyBase< flxDevSCD30, false, false >, _flxPropertyBase< flxDevSCD40, false, false >, _flxPropertyBase< flxDevSDP3X, false, false >, _flxPropertyBase< flxDevSEN54, false, false >, _flxPropertyBase< flxDevSTC31, false, false >, _flxPropertyBase< flxDevSTHS34PF80, false, false >, _flxPropertyBase< flxDevSerial, false, false >, _flxPropertyBase< flxDevSoilMoisture, false, false >, _flxPropertyBase< flxDevTMF882X, false, false >, _flxPropertyBase< flxDevTwist, false, false >, _flxPropertyBase< flxDevVCNL4040, false, false >, _flxPropertyBase< flxDevVEML6075, false, false >, _flxPropertyBase< flxDevVEML7700, false, false >, _flxPropertyBase< flxDevVL53L1X, false, false >, _flxPropertyBase< flxDevVL53L5, false, false >, _flxPropertyBase< flxFileRotate, false, false >, _flxPropertyBase< flxIoTArduino, false, false >, _flxPropertyBase< flxLogger, false, false >, _flxPropertyBase< flxOptEnableDevice, false, false >, _flxPropertyBase< flxOptExtSerial, false, false >, _flxPropertyBase< flxOptInterruptEvent, false, false >, _flxPropertyBase< flxSettingsSave, false, false >, _flxPropertyBase< flxTimer, false, false >, _flxPropertyBaseString< HIDDEN, SECURE >, and _flxPropertyBaseString< false, false >.

◆ size()

virtual size_t flxProperty::size ( void  )
inlinevirtual

Reimplemented in _flxPropertyBase< T, HIDDEN, SECURE >, _flxPropertyBase< T, false, false >, _flxPropertyBase< _flxClock, false, false >, _flxPropertyBase< flxDevACS37800, false, false >, _flxPropertyBase< flxDevADS1015, false, false >, _flxPropertyBase< flxDevADS122C04, false, false >, _flxPropertyBase< flxDevAMG8833, false, false >, _flxPropertyBase< flxDevAS7265X, false, false >, _flxPropertyBase< flxDevAS7331, false, false >, _flxPropertyBase< flxDevAS7343, false, false >, _flxPropertyBase< flxDevAnalogPin, false, false >, _flxPropertyBase< flxDevBMP581, false, false >, _flxPropertyBase< flxDevBMV080, false, false >, _flxPropertyBase< flxDevButton, false, false >, _flxPropertyBase< flxDevENS160, false, false >, _flxPropertyBase< flxDevFS3000, false, false >, _flxPropertyBase< flxDevGNSS, false, false >, _flxPropertyBase< flxDevISM330Base, false, false >, _flxPropertyBase< flxDevMCP9600, false, false >, _flxPropertyBase< flxDevMMC5983Base, false, false >, _flxPropertyBase< flxDevNAU7802, false, false >, _flxPropertyBase< flxDevOPT4048, false, false >, _flxPropertyBase< flxDevPASCO2V01, false, false >, _flxPropertyBase< flxDevSCD30, false, false >, _flxPropertyBase< flxDevSCD40, false, false >, _flxPropertyBase< flxDevSDP3X, false, false >, _flxPropertyBase< flxDevSEN54, false, false >, _flxPropertyBase< flxDevSTC31, false, false >, _flxPropertyBase< flxDevSTHS34PF80, false, false >, _flxPropertyBase< flxDevSerial, false, false >, _flxPropertyBase< flxDevSoilMoisture, false, false >, _flxPropertyBase< flxDevTMF882X, false, false >, _flxPropertyBase< flxDevTwist, false, false >, _flxPropertyBase< flxDevVCNL4040, false, false >, _flxPropertyBase< flxDevVEML6075, false, false >, _flxPropertyBase< flxDevVEML7700, false, false >, _flxPropertyBase< flxDevVL53L1X, false, false >, _flxPropertyBase< flxDevVL53L5, false, false >, _flxPropertyBase< flxFileRotate, false, false >, _flxPropertyBase< flxIoTArduino, false, false >, _flxPropertyBase< flxLogger, false, false >, _flxPropertyBase< flxOptEnableDevice, false, false >, _flxPropertyBase< flxOptExtSerial, false, false >, _flxPropertyBase< flxOptInterruptEvent, false, false >, _flxPropertyBase< flxSettingsSave, false, false >, _flxPropertyBase< flxTimer, false, false >, _flxPropertyBaseString< HIDDEN, SECURE >, and _flxPropertyBaseString< false, false >.

◆ to_string()

virtual std::string flxProperty::to_string ( void  )
inlinevirtual

Reimplemented in _flxPropertyBaseString< HIDDEN, SECURE >, _flxPropertyBaseString< false, false >, _flxPropertyBase< T, HIDDEN, SECURE >, _flxPropertyBase< T, false, false >, _flxPropertyBase< _flxClock, false, false >, _flxPropertyBase< flxDevACS37800, false, false >, _flxPropertyBase< flxDevADS1015, false, false >, _flxPropertyBase< flxDevADS122C04, false, false >, _flxPropertyBase< flxDevAMG8833, false, false >, _flxPropertyBase< flxDevAS7265X, false, false >, _flxPropertyBase< flxDevAS7331, false, false >, _flxPropertyBase< flxDevAS7343, false, false >, _flxPropertyBase< flxDevAnalogPin, false, false >, _flxPropertyBase< flxDevBMP581, false, false >, _flxPropertyBase< flxDevBMV080, false, false >, _flxPropertyBase< flxDevButton, false, false >, _flxPropertyBase< flxDevENS160, false, false >, _flxPropertyBase< flxDevFS3000, false, false >, _flxPropertyBase< flxDevGNSS, false, false >, _flxPropertyBase< flxDevISM330Base, false, false >, _flxPropertyBase< flxDevMCP9600, false, false >, _flxPropertyBase< flxDevMMC5983Base, false, false >, _flxPropertyBase< flxDevNAU7802, false, false >, _flxPropertyBase< flxDevOPT4048, false, false >, _flxPropertyBase< flxDevPASCO2V01, false, false >, _flxPropertyBase< flxDevSCD30, false, false >, _flxPropertyBase< flxDevSCD40, false, false >, _flxPropertyBase< flxDevSDP3X, false, false >, _flxPropertyBase< flxDevSEN54, false, false >, _flxPropertyBase< flxDevSTC31, false, false >, _flxPropertyBase< flxDevSTHS34PF80, false, false >, _flxPropertyBase< flxDevSerial, false, false >, _flxPropertyBase< flxDevSoilMoisture, false, false >, _flxPropertyBase< flxDevTMF882X, false, false >, _flxPropertyBase< flxDevTwist, false, false >, _flxPropertyBase< flxDevVCNL4040, false, false >, _flxPropertyBase< flxDevVEML6075, false, false >, _flxPropertyBase< flxDevVEML7700, false, false >, _flxPropertyBase< flxDevVL53L1X, false, false >, _flxPropertyBase< flxDevVL53L5, false, false >, _flxPropertyBase< flxFileRotate, false, false >, _flxPropertyBase< flxIoTArduino, false, false >, _flxPropertyBase< flxLogger, false, false >, _flxPropertyBase< flxOptEnableDevice, false, false >, _flxPropertyBase< flxOptExtSerial, false, false >, _flxPropertyBase< flxOptInterruptEvent, false, false >, _flxPropertyBase< flxSettingsSave, false, false >, and _flxPropertyBase< flxTimer, false, false >.

◆ type()

virtual flxDataType_t flxProperty::type ( void  )
pure virtual

Implemented in _flxPropertyBase< T, HIDDEN, SECURE >, _flxPropertyBase< T, false, false >, _flxPropertyBase< _flxClock, false, false >, _flxPropertyBase< flxDevACS37800, false, false >, _flxPropertyBase< flxDevADS1015, false, false >, _flxPropertyBase< flxDevADS122C04, false, false >, _flxPropertyBase< flxDevAMG8833, false, false >, _flxPropertyBase< flxDevAS7265X, false, false >, _flxPropertyBase< flxDevAS7331, false, false >, _flxPropertyBase< flxDevAS7343, false, false >, _flxPropertyBase< flxDevAnalogPin, false, false >, _flxPropertyBase< flxDevBMP581, false, false >, _flxPropertyBase< flxDevBMV080, false, false >, _flxPropertyBase< flxDevButton, false, false >, _flxPropertyBase< flxDevENS160, false, false >, _flxPropertyBase< flxDevFS3000, false, false >, _flxPropertyBase< flxDevGNSS, false, false >, _flxPropertyBase< flxDevISM330Base, false, false >, _flxPropertyBase< flxDevMCP9600, false, false >, _flxPropertyBase< flxDevMMC5983Base, false, false >, _flxPropertyBase< flxDevNAU7802, false, false >, _flxPropertyBase< flxDevOPT4048, false, false >, _flxPropertyBase< flxDevPASCO2V01, false, false >, _flxPropertyBase< flxDevSCD30, false, false >, _flxPropertyBase< flxDevSCD40, false, false >, _flxPropertyBase< flxDevSDP3X, false, false >, _flxPropertyBase< flxDevSEN54, false, false >, _flxPropertyBase< flxDevSTC31, false, false >, _flxPropertyBase< flxDevSTHS34PF80, false, false >, _flxPropertyBase< flxDevSerial, false, false >, _flxPropertyBase< flxDevSoilMoisture, false, false >, _flxPropertyBase< flxDevTMF882X, false, false >, _flxPropertyBase< flxDevTwist, false, false >, _flxPropertyBase< flxDevVCNL4040, false, false >, _flxPropertyBase< flxDevVEML6075, false, false >, _flxPropertyBase< flxDevVEML7700, false, false >, _flxPropertyBase< flxDevVL53L1X, false, false >, _flxPropertyBase< flxDevVL53L5, false, false >, _flxPropertyBase< flxFileRotate, false, false >, _flxPropertyBase< flxIoTArduino, false, false >, _flxPropertyBase< flxLogger, false, false >, _flxPropertyBase< flxOptEnableDevice, false, false >, _flxPropertyBase< flxOptExtSerial, false, false >, _flxPropertyBase< flxOptInterruptEvent, false, false >, _flxPropertyBase< flxSettingsSave, false, false >, _flxPropertyBase< flxTimer, false, false >, _flxPropertyBaseString< HIDDEN, SECURE >, and _flxPropertyBaseString< false, false >.


The documentation for this class was generated from the following file: