flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxStorageOld Class Referenceabstract

#include <flxStorage.h>

Public Member Functions

virtual flxStorageBlockOld * beginBlock (uint16_t idBlock, size_t sz)=0
 
virtual flxStorageBlockOld * getBlock (uint16_t idBlock)=0
 
virtual void endBlock (flxStorageBlockOld *)=0
 
virtual void resetStorage ()=0
 

Member Function Documentation

◆ beginBlock()

virtual flxStorageBlockOld * flxStorageOld::beginBlock ( uint16_t  idBlock,
size_t  sz 
)
pure virtual

◆ endBlock()

virtual void flxStorageOld::endBlock ( flxStorageBlockOld *  )
pure virtual

◆ getBlock()

virtual flxStorageBlockOld * flxStorageOld::getBlock ( uint16_t  idBlock)
pure virtual

◆ resetStorage()

virtual void flxStorageOld::resetStorage ( )
pure virtual

The documentation for this class was generated from the following file: