![]() |
flux sdk
v01.05.00-6-g190c94c
Embedded C++ SDK
|
This is the complete list of members for flxWriter, including all inherited members.
| colorEnabled(void) | flxWriter | inlinevirtual |
| textToBlue(void) | flxWriter | inlinevirtual |
| textToCyan(void) | flxWriter | inlinevirtual |
| textToGreen(void) | flxWriter | inlinevirtual |
| textToMagenta(void) | flxWriter | inlinevirtual |
| textToNormal(void) | flxWriter | inlinevirtual |
| textToRed(void) | flxWriter | inlinevirtual |
| textToWhite(void) | flxWriter | inlinevirtual |
| textToYellow(void) | flxWriter | inlinevirtual |
| write(bool value) | flxWriter | inlinevirtual |
| write(int32_t)=0 | flxWriter | pure virtual |
| write(float)=0 | flxWriter | pure virtual |
| write(const char *value, bool newline, flxLineType_t type)=0 | flxWriter | pure virtual |
| write(const char *value, bool newline) | flxWriter | inlinevirtual |
| write(std::string &value, bool newline) | flxWriter | inlinevirtual |
| write(const char *value) | flxWriter | inlinevirtual |
| write(std::string &value) | flxWriter | inlinevirtual |