flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxWriter Class Referenceabstract

#include <flxCoreInterface.h>

Inheritance diagram for flxWriter:
flxFileRotate flxIoTAWS flxIoTAzure flxSerial_

Public Member Functions

virtual void write (bool value)
 
virtual void write (int32_t)=0
 
virtual void write (float)=0
 
virtual void write (const char *value, bool newline, flxLineType_t type)=0
 
virtual void write (const char *value, bool newline)
 
virtual void write (std::string &value, bool newline)
 
virtual void write (const char *value)
 
virtual void write (std::string &value)
 
virtual bool colorEnabled (void)
 
virtual void textToRed (void)
 
virtual void textToGreen (void)
 
virtual void textToYellow (void)
 
virtual void textToBlue (void)
 
virtual void textToWhite (void)
 
virtual void textToNormal (void)
 
virtual void textToCyan (void)
 
virtual void textToMagenta (void)
 

Member Function Documentation

◆ colorEnabled()

virtual bool flxWriter::colorEnabled ( void  )
inlinevirtual

Reimplemented in flxSerial_.

◆ textToBlue()

virtual void flxWriter::textToBlue ( void  )
inlinevirtual

Reimplemented in flxSerial_.

◆ textToCyan()

virtual void flxWriter::textToCyan ( void  )
inlinevirtual

Reimplemented in flxSerial_.

◆ textToGreen()

virtual void flxWriter::textToGreen ( void  )
inlinevirtual

Reimplemented in flxSerial_.

◆ textToMagenta()

virtual void flxWriter::textToMagenta ( void  )
inlinevirtual

Reimplemented in flxSerial_.

◆ textToNormal()

virtual void flxWriter::textToNormal ( void  )
inlinevirtual

Reimplemented in flxSerial_.

◆ textToRed()

virtual void flxWriter::textToRed ( void  )
inlinevirtual

Reimplemented in flxSerial_.

◆ textToWhite()

virtual void flxWriter::textToWhite ( void  )
inlinevirtual

Reimplemented in flxSerial_.

◆ textToYellow()

virtual void flxWriter::textToYellow ( void  )
inlinevirtual

Reimplemented in flxSerial_.

◆ write() [1/8]

virtual void flxWriter::write ( bool  value)
inlinevirtual

◆ write() [2/8]

virtual void flxWriter::write ( const char *  value)
inlinevirtual

◆ write() [3/8]

virtual void flxWriter::write ( const char *  value,
bool  newline 
)
inlinevirtual

◆ write() [4/8]

virtual void flxWriter::write ( const char *  value,
bool  newline,
flxLineType_t  type 
)
pure virtual

◆ write() [5/8]

virtual void flxWriter::write ( float  )
pure virtual

◆ write() [6/8]

virtual void flxWriter::write ( int32_t  )
pure virtual

◆ write() [7/8]

virtual void flxWriter::write ( std::string &  value)
inlinevirtual

◆ write() [8/8]

virtual void flxWriter::write ( std::string &  value,
bool  newline 
)
inlinevirtual

The documentation for this class was generated from the following file: