flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxIoTAzure Class Reference

#include <flxIoTAzure.h>

Inheritance diagram for flxIoTAzure:
flxWriter

Public Member Functions

 flxIoTAzure ()
 
void write (int32_t data)
 
void write (float data)
 
virtual void write (const char *value, bool newline, flxLineType_t type)
 
bool initializeIoTHubClient ()
 
bool connect ()
 
void disconnect ()
 
bool initialize (void)
 
void jobHandlerCB (void)
 
- Public Member Functions inherited from flxWriter
virtual void write (bool value)
 
virtual void write (int32_t)=0
 
virtual void write (float)=0
 
virtual void write (const char *value, bool newline, flxLineType_t type)=0
 
virtual void write (const char *value, bool newline)
 
virtual void write (std::string &value, bool newline)
 
virtual void write (const char *value)
 
virtual void write (std::string &value)
 
virtual bool colorEnabled (void)
 
virtual void textToRed (void)
 
virtual void textToGreen (void)
 
virtual void textToYellow (void)
 
virtual void textToBlue (void)
 
virtual void textToWhite (void)
 
virtual void textToNormal (void)
 
virtual void textToCyan (void)
 
virtual void textToMagenta (void)
 

Public Attributes

flxPropertyString< flxIoTAzure > deviceID
 
flxPropertySecureString< flxIoTAzure > deviceKey
 

Constructor & Destructor Documentation

◆ flxIoTAzure()

flxIoTAzure::flxIoTAzure ( )
inline

Member Function Documentation

◆ connect()

bool flxIoTAzure::connect ( )
inline

◆ disconnect()

void flxIoTAzure::disconnect ( )
inline

◆ initialize()

bool flxIoTAzure::initialize ( void  )
inline

◆ initializeIoTHubClient()

bool flxIoTAzure::initializeIoTHubClient ( )
inline

◆ jobHandlerCB()

void flxIoTAzure::jobHandlerCB ( void  )
inline

◆ write() [1/3]

virtual void flxIoTAzure::write ( const char *  value,
bool  newline,
flxLineType_t  type 
)
inlinevirtual

Implements flxWriter.

◆ write() [2/3]

void flxIoTAzure::write ( float  data)
inlinevirtual

Implements flxWriter.

◆ write() [3/3]

void flxIoTAzure::write ( int32_t  data)
inlinevirtual

Implements flxWriter.

Member Data Documentation

◆ deviceID

flxPropertyString<flxIoTAzure> flxIoTAzure::deviceID

◆ deviceKey

flxPropertySecureString<flxIoTAzure> flxIoTAzure::deviceKey

The documentation for this class was generated from the following file: