flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxIoTAzure Member List

This is the complete list of members for flxIoTAzure, including all inherited members.

colorEnabled(void)flxWriterinlinevirtual
connect()flxIoTAzureinline
deviceIDflxIoTAzure
deviceKeyflxIoTAzure
disconnect()flxIoTAzureinline
flxIoTAzure()flxIoTAzureinline
initialize(void)flxIoTAzureinline
initializeIoTHubClient()flxIoTAzureinline
jobHandlerCB(void)flxIoTAzureinline
textToBlue(void)flxWriterinlinevirtual
textToCyan(void)flxWriterinlinevirtual
textToGreen(void)flxWriterinlinevirtual
textToMagenta(void)flxWriterinlinevirtual
textToNormal(void)flxWriterinlinevirtual
textToRed(void)flxWriterinlinevirtual
textToWhite(void)flxWriterinlinevirtual
textToYellow(void)flxWriterinlinevirtual
write(int32_t data)flxIoTAzureinlinevirtual
write(float data)flxIoTAzureinlinevirtual
write(const char *value, bool newline, flxLineType_t type)flxIoTAzureinlinevirtual
flxWriter::write(bool value)flxWriterinlinevirtual
flxWriter::write(const char *value, bool newline)flxWriterinlinevirtual
flxWriter::write(std::string &value, bool newline)flxWriterinlinevirtual
flxWriter::write(const char *value)flxWriterinlinevirtual
flxWriter::write(std::string &value)flxWriterinlinevirtual