Skip to main content

SparkFun MCP4725 Arduino Library

!!! note "Arduino" This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino IDE, library, or board add-on, please review the following tutorials.

Installing the SparkFun ADS1219 Arduino Library​

!!! note "SparkFun Toolkit"

This library is built using the SparkFun Toolkit so you'll need to make sure that is installed before using this library. Install the SparkFun Toolkit with the Arduino Library manager by searching "SparkFun Toolkit" and installing the latest version. Users who prefer manually installing Arduino Libraries can download it from the GitHub Repository.

Library Setup​

The SparkFun MCP4725 Arduino Library lets users easily get started with the MCP4725 with basic commands and includes seven examples. Install the library using the Arduino Library Manager tool by searching for "SparkFun MCP4725" and install the latest version. If you'd prefer to manually install the library, you can download it from the GitHub Repository or you can download a ZIP of the repository here.