Skip to main content

Hardware Assembly

Basic USB Assembly​

Basic assembly of the Thing Plus ESP32-C5 only requires a USB-C cable connecting the board to a computer. Just plug the cable into the USB-C connector like the photo below shows and you should see the RGB LED cycling through rainbow colors with the pre-loaded test code. From here, we can move on to working with the included MicroPython examples or installing the espressif boards package in the Arduino IDE.

The Thing Plus - ESP32-C5 connected over USB-C

The Thing Plus - ESP32-C5 connected over USB-C

Battery Assembly​

If you prefer a battery-powered application, plug a single-cell LiPo battery into the 2-pin JST connector on the underside of the board like the photo below. Remember, the MCP73831 only charges the battery when V_USB has voltage present either from the USB-C connector or through the V_USB PTH pin.