flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxDataArrayString Member List

This is the complete list of members for flxDataArrayString, including all inherited members.

_bAllocflxDataArrayType< char * >protected
_dimensionsflxDataArrayprotected
_n_dimsflxDataArrayprotected
dimensions()flxDataArrayinline
flxDataArray()flxDataArrayinline
flxDataArrayType()flxDataArrayType< char * >inline
get()flxDataArrayType< char * >inline
kMaxArrayDimsflxDataArrayprotectedstatic
n_dimensions()flxDataArrayinline
reset()flxDataArrayType< char * >inlineprotectedvirtual
set(char * *data, uint16_t d0, bool no_copy=false)flxDataArrayType< char * >inline
set(char * *data, uint16_t d0, uint16_t d1, bool no_copy=false)flxDataArrayType< char * >inline
set(char * *data, uint16_t d0, uint16_t d1, uint16_t d2, bool no_copy=false)flxDataArrayType< char * >inline
setDimensions(uint16_t d0)flxDataArrayinlineprotected
setDimensions(uint16_t d0, uint16_t d1)flxDataArrayinlineprotected
setDimensions(uint16_t d0, uint16_t d1, uint16_t d2)flxDataArrayinlineprotected
size(void)flxDataArrayinline
type(void)flxDataArrayType< char * >inlinevirtual
~flxDataArray()flxDataArrayinlinevirtual
~flxDataArrayType()flxDataArrayType< char * >inline