flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxDataArrayType< T > Class Template Reference

A templated class to define an array class of a specific type. More...

#include <flxCoreTypes.h>

Inheritance diagram for flxDataArrayType< T >:
flxDataArray

Public Member Functions

 flxDataArrayType ()
 
 ~flxDataArrayType ()
 
flxDataType_t type (void)
 Return the data type of the array. More...
 
void set (T *data, uint16_t d0, bool no_copy=false)
 Set the array data and pass in dimensions for the array. More...
 
void set (T *data, uint16_t d0, uint16_t d1, bool no_copy=false)
 Set the array data and pass in dimensions for the array. More...
 
void set (T *data, uint16_t d0, uint16_t d1, uint16_t d2, bool no_copy=false)
 Set the array data and pass in dimensions for the array. More...
 
T * get ()
 Return a pointer to the array data. More...
 
- Public Member Functions inherited from flxDataArray
 flxDataArray ()
 
virtual ~flxDataArray ()
 
virtual flxDataType_t type ()=0
 
uint8_t n_dimensions ()
 Return the number of dimensions in the array. More...
 
uint16_t * dimensions ()
 Return a pointer to the array's dimensions array . More...
 
size_t size (void)
 Return the total number of elements in the array. More...
 

Protected Member Functions

virtual void reset ()
 
virtual void freeAlloc (void)
 
virtual bool setDataPtr (T *data, size_t length, bool no_copy)
 
- Protected Member Functions inherited from flxDataArray
void setDimensions (uint16_t d0)
 
void setDimensions (uint16_t d0, uint16_t d1)
 
void setDimensions (uint16_t d0, uint16_t d1, uint16_t d2)
 
virtual void reset ()
 

Protected Attributes

bool _bAlloc
 
- Protected Attributes inherited from flxDataArray
uint8_t _n_dims
 
uint16_t _dimensions [kMaxArrayDims]
 

Additional Inherited Members

- Static Protected Attributes inherited from flxDataArray
static constexpr uint16_t kMaxArrayDims = 3
 

Detailed Description

template<typename T>
class flxDataArrayType< T >

A templated class to define an array class of a specific type.

Constructor & Destructor Documentation

◆ flxDataArrayType()

template<typename T >
flxDataArrayType< T >::flxDataArrayType ( )
inline

◆ ~flxDataArrayType()

template<typename T >
flxDataArrayType< T >::~flxDataArrayType ( )
inline

Member Function Documentation

◆ freeAlloc()

template<typename T >
virtual void flxDataArrayType< T >::freeAlloc ( void  )
inlineprotectedvirtual

◆ get()

template<typename T >
T * flxDataArrayType< T >::get ( )
inline

Return a pointer to the array data.

Returns
T* Templated type pointer

◆ reset()

template<typename T >
virtual void flxDataArrayType< T >::reset ( )
inlineprotectedvirtual

Reimplemented from flxDataArray.

◆ set() [1/3]

template<typename T >
void flxDataArrayType< T >::set ( T *  data,
uint16_t  d0,
bool  no_copy = false 
)
inline

Set the array data and pass in dimensions for the array.

Parameters
dataThe array data pointer
d0The first dimension of the array
no_copyIf set, the data is not copied.

◆ set() [2/3]

template<typename T >
void flxDataArrayType< T >::set ( T *  data,
uint16_t  d0,
uint16_t  d1,
bool  no_copy = false 
)
inline

Set the array data and pass in dimensions for the array.

Parameters
dataThe array data pointer
d0The first dimension of the array
d1The second dimension of the array
no_copyIf set, the data is not copied.

◆ set() [3/3]

template<typename T >
void flxDataArrayType< T >::set ( T *  data,
uint16_t  d0,
uint16_t  d1,
uint16_t  d2,
bool  no_copy = false 
)
inline

Set the array data and pass in dimensions for the array.

Parameters
dataThe array data pointer
d0The first dimension of the array
d1The second dimension of the array
d2The third dimension of the array
no_copyIf set, the data is not copied.

◆ setDataPtr()

template<typename T >
virtual bool flxDataArrayType< T >::setDataPtr ( T *  data,
size_t  length,
bool  no_copy 
)
inlineprotectedvirtual

◆ type()

template<typename T >
flxDataType_t flxDataArrayType< T >::type ( void  )
inlinevirtual

Return the data type of the array.

Returns
flxDataType_t

Implements flxDataArray.

Member Data Documentation

◆ _bAlloc

template<typename T >
bool flxDataArrayType< T >::_bAlloc
protected

The documentation for this class was generated from the following file: