flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxDataArrayType< T > Member List

This is the complete list of members for flxDataArrayType< T >, including all inherited members.

_bAllocflxDataArrayType< T >protected
_dimensionsflxDataArrayprotected
_n_dimsflxDataArrayprotected
dimensions()flxDataArrayinline
flxDataArray()flxDataArrayinline
flxDataArrayType()flxDataArrayType< T >inline
freeAlloc(void)flxDataArrayType< T >inlineprotectedvirtual
get()flxDataArrayType< T >inline
kMaxArrayDimsflxDataArrayprotectedstatic
n_dimensions()flxDataArrayinline
reset()flxDataArrayType< T >inlineprotectedvirtual
set(T *data, uint16_t d0, bool no_copy=false)flxDataArrayType< T >inline
set(T *data, uint16_t d0, uint16_t d1, bool no_copy=false)flxDataArrayType< T >inline
set(T *data, uint16_t d0, uint16_t d1, uint16_t d2, bool no_copy=false)flxDataArrayType< T >inline
setDataPtr(T *data, size_t length, bool no_copy)flxDataArrayType< T >inlineprotectedvirtual
setDimensions(uint16_t d0)flxDataArrayinlineprotected
setDimensions(uint16_t d0, uint16_t d1)flxDataArrayinlineprotected
setDimensions(uint16_t d0, uint16_t d1, uint16_t d2)flxDataArrayinlineprotected
size(void)flxDataArrayinline
type(void)flxDataArrayType< T >inlinevirtual
~flxDataArray()flxDataArrayinlinevirtual
~flxDataArrayType()flxDataArrayType< T >inline