flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxDataArray Class Referenceabstract

This class is used as a base class for the templated array classes. More...

#include <flxCoreTypes.h>

Inheritance diagram for flxDataArray:
flxDataArrayType< char * > flxDataArrayType< T > flxDataArrayString

Public Member Functions

 flxDataArray ()
 
virtual ~flxDataArray ()
 
virtual flxDataType_t type ()=0
 
uint8_t n_dimensions ()
 Return the number of dimensions in the array. More...
 
uint16_t * dimensions ()
 Return a pointer to the array's dimensions array . More...
 
size_t size (void)
 Return the total number of elements in the array. More...
 

Protected Member Functions

void setDimensions (uint16_t d0)
 
void setDimensions (uint16_t d0, uint16_t d1)
 
void setDimensions (uint16_t d0, uint16_t d1, uint16_t d2)
 
virtual void reset ()
 

Protected Attributes

uint8_t _n_dims
 
uint16_t _dimensions [kMaxArrayDims]
 

Static Protected Attributes

static constexpr uint16_t kMaxArrayDims = 3
 

Detailed Description

This class is used as a base class for the templated array classes.

Note
Currently the interface only supports up to 3 dimensions.

Constructor & Destructor Documentation

◆ flxDataArray()

flxDataArray::flxDataArray ( )
inline

◆ ~flxDataArray()

virtual flxDataArray::~flxDataArray ( )
inlinevirtual

Member Function Documentation

◆ dimensions()

uint16_t * flxDataArray::dimensions ( )
inline

Return a pointer to the array's dimensions array .

Returns
uint16_t*

◆ n_dimensions()

uint8_t flxDataArray::n_dimensions ( )
inline

Return the number of dimensions in the array.

Returns
uint8_t

◆ reset()

virtual void flxDataArray::reset ( )
inlineprotectedvirtual

◆ setDimensions() [1/3]

void flxDataArray::setDimensions ( uint16_t  d0)
inlineprotected

◆ setDimensions() [2/3]

void flxDataArray::setDimensions ( uint16_t  d0,
uint16_t  d1 
)
inlineprotected

◆ setDimensions() [3/3]

void flxDataArray::setDimensions ( uint16_t  d0,
uint16_t  d1,
uint16_t  d2 
)
inlineprotected

◆ size()

size_t flxDataArray::size ( void  )
inline

Return the total number of elements in the array.

Returns
size_t

◆ type()

virtual flxDataType_t flxDataArray::type ( )
pure virtual

Member Data Documentation

◆ _dimensions

uint16_t flxDataArray::_dimensions[kMaxArrayDims]
protected

◆ _n_dims

uint8_t flxDataArray::_n_dims
protected

◆ kMaxArrayDims

constexpr uint16_t flxDataArray::kMaxArrayDims = 3
staticconstexprprotected

The documentation for this class was generated from the following file: