flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxFSSDFile Class Reference

#include <flxFSSDCard.h>

Inheritance diagram for flxFSSDFile:
flxIFile

Public Member Functions

 flxFSSDFile ()
 
size_t write (const uint8_t *buf, size_t size)
 
size_t read (uint8_t *buf, size_t size)
 
void close (void)
 
bool isValid (void)
 
void flush (void)
 
size_t size (void)
 
const char * name (void)
 
bool isDirectory (void)
 
std::string getNextFilename (void)
 
int available (void)
 
Stream * stream (void)
 
flxFSFile openNextFile (void)
 
time_t getLastWrite (void)
 
File filePointer (void)
 
virtual size_t write (const uint8_t *buf, size_t size)=0
 
virtual void close (void)=0
 
virtual bool isValid (void)=0
 
virtual void flush (void)=0
 
virtual size_t size (void)=0
 
virtual size_t read (uint8_t *buf, size_t size)=0
 
virtual const char * name (void)=0
 
virtual bool isDirectory (void)=0
 
virtual std::string getNextFilename (void)=0
 
virtual int available (void)=0
 
virtual Stream * stream (void)=0
 
virtual flxFSFile openNextFile (void)=0
 
virtual time_t getLastWrite (void)=0
 
virtual File filePointer (void)=0
 

Constructor & Destructor Documentation

◆ flxFSSDFile()

flxFSSDFile::flxFSSDFile ( )
inline

Member Function Documentation

◆ available()

int flxFSSDFile::available ( void  )
virtual

Implements flxIFile.

◆ close()

void flxFSSDFile::close ( void  )
virtual

Implements flxIFile.

◆ filePointer()

File flxFSSDFile::filePointer ( void  )
inlinevirtual

Implements flxIFile.

◆ flush()

void flxFSSDFile::flush ( void  )
virtual

Implements flxIFile.

◆ getLastWrite()

time_t flxFSSDFile::getLastWrite ( void  )
virtual

Implements flxIFile.

◆ getNextFilename()

std::string flxFSSDFile::getNextFilename ( void  )
virtual

Implements flxIFile.

◆ isDirectory()

bool flxFSSDFile::isDirectory ( void  )
virtual

Implements flxIFile.

◆ isValid()

bool flxFSSDFile::isValid ( void  )
virtual

Implements flxIFile.

◆ name()

const char * flxFSSDFile::name ( void  )
virtual

Implements flxIFile.

◆ openNextFile()

flxFSFile flxFSSDFile::openNextFile ( void  )
virtual

Implements flxIFile.

◆ read()

size_t flxFSSDFile::read ( uint8_t *  buf,
size_t  size 
)
virtual

Implements flxIFile.

◆ size()

size_t flxFSSDFile::size ( void  )
virtual

Implements flxIFile.

◆ stream()

Stream * flxFSSDFile::stream ( void  )
virtual

Implements flxIFile.

◆ write()

size_t flxFSSDFile::write ( const uint8_t *  buf,
size_t  size 
)
virtual

Implements flxIFile.


The documentation for this class was generated from the following files: