flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxIClock Class Referenceabstract

#include <flxClock.h>

Inheritance diagram for flxIClock:
flxDevGNSS flxDevRV8803 flxISystemClock

Public Member Functions

virtual uint32_t get_epoch (void)=0
 
virtual void set_epoch (const uint32_t &)=0
 
virtual bool valid_epoch (void)=0
 

Member Function Documentation

◆ get_epoch()

virtual uint32_t flxIClock::get_epoch ( void  )
pure virtual

Implemented in flxDevGNSS, and flxDevRV8803.

◆ set_epoch()

virtual void flxIClock::set_epoch ( const uint32_t &  )
pure virtual

Implemented in flxDevRV8803, and flxDevGNSS.

◆ valid_epoch()

virtual bool flxIClock::valid_epoch ( void  )
pure virtual

Implemented in flxDevGNSS, and flxDevRV8803.


The documentation for this class was generated from the following file: