flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxDevGNSS Class Reference

#include <flxDevGNSS.h>

Inheritance diagram for flxDevGNSS:
flxDeviceI2CType< flxDevGNSS > flxIClock flxDevice flxOperation flxObject _flxParameterContainer flxPersist _flxPropertyContainer flxDescriptor

Public Member Functions

 flxDevGNSS ()
 
bool onInitialize (TwoWire &)
 
void setAvailablePPSPins (const uint16_t *ppsPin, size_t len)
 
uint32_t get_epoch (void)
 
void set_epoch (const uint32_t &refEpoch)
 
bool valid_epoch (void)
 
- Public Member Functions inherited from flxDeviceI2CType< flxDevGNSS >
virtual uint8_t getDefaultAddress (void)
 
bool initialize (TwoWire &wirePort)
 
bool initialize (flxBusI2C &i2cDriver)
 
bool initialize (void)
 
bool initialize (uint8_t address)
 
virtual bool onInitialize (TwoWire &)
 
flxTypeID getType (void)
 
bool isType (flxTypeID type)
 
flxDeviceKind_t getKind (void)
 
- Public Member Functions inherited from flxDevice
 flxDevice ()
 
virtual ~flxDevice ()
 
virtual bool execute (void)
 Virtual method called to run the operation - called before data is retrieved. More...
 
bool initialize ()
 
virtual bool initialize (flxBusI2C &)
 
virtual bool initialize (flxBusSPI &)
 
bool autoload (void)
 
void setAutoload ()
 
void setAddress (uint8_t address)
 
uint8_t address (void)
 
void addAddressToName ()
 
void setIsInitialized (bool isInit)
 
bool isInitialized (void)
 
virtual flxDeviceKind_t getKind (void)
 
- Public Member Functions inherited from flxOperation
virtual flxTypeID getType (void)
 
virtual bool execute (void)
 Virtual method called to run the operation - called before data is retrieved. More...
 
virtual bool onSave (flxStorageBlock *stBlk)
 
virtual bool onRestore (flxStorageBlock *stBlk)
 
- Public Member Functions inherited from flxObject
 flxObject ()
 
virtual ~flxObject ()
 
virtual size_t n_children (void)
 
void setParent (flxObject *parent)
 
void setParent (flxObject &parent)
 
flxObject * parent ()
 
void setHidden (bool bHide=true)
 
bool hidden ()
 
void setIsDirty (bool bDirty=true)
 
bool isDirty (void)
 
virtual bool onSave (flxStorageBlock *stBlk)
 
virtual bool save (flxStorage *pStorage)
 
virtual void restoreComplete (void)
 
virtual bool onRestore (flxStorageBlock *stBlk)
 
virtual bool restore (flxStorage *pStorage)
 
virtual flxTypeID getType (void)
 
virtual bool save (flxStorage *)=0
 
virtual bool restore (flxStorage *)=0
 
- Public Member Functions inherited from _flxPropertyContainer
 _flxPropertyContainer ()
 
void addProperty (flxProperty *newProperty)
 
void addProperty (flxProperty &newProperty)
 
void removeProperty (flxProperty *rmProp)
 
bool containsProperty (flxProperty *prop)
 
void removeProperty (flxProperty &rmProp)
 
flxPropertyList & getProperties (void)
 
uint nProperties (void)
 
bool saveProperties (flxStorageBlock *stBlk)
 
bool restoreProperties (flxStorageBlock *stBlk)
 
size_t propertySaveSize ()
 
void hideProperty (flxProperty &theProp)
 
- Public Member Functions inherited from flxDescriptor
 flxDescriptor ()
 
void setName (const char *new_name)
 Set the Name object - storing the pointer to the provided string No allocation is performed. If the previous name was allocated, it is freed. More...
 
void setName (const char *new_name, const char *new_desc)
 Set the Name object and the Description for the object. Both strings are constants. More...
 
void setName (char *new_name)
 Set the Name object, but makes a copy of the input string since the input is not const. If the previous name was allocated, it is freed. More...
 
const char * name ()
 Return a const char pointer to the name of the object. More...
 
std::string name_ (void)
 Returns a std::string of the name of the object. More...
 
void setDescription (const char *new_desc)
 Set the Description object - the input value is constant and not copied. If the previous description was allocated, it is freed. More...
 
void setDescription (char *new_desc)
 Set the Description object - the input value is not constant and is copied. If the previous description was allocated, it is freed. More...
 
const char * description ()
 Return the constant C string pointer to the description of the object. More...
 
std::string description_ (void)
 Return the description of the object as a std::string. More...
 
void setTitle (const char *title)
 Set the Title object - the title is optional and is used mostly for UX or organizational purposes. The input value is constant and not copied. If the previous title was allocated, it is freed. More...
 
void setTitleAlloc (char *new_title)
 Set the Title of the object , but make an explict copy of the provided string. More...
 
const char * title (void)
 Return the C constant string pointer to the title of the object. More...
 
- Public Member Functions inherited from _flxParameterContainer
void addParameter (flxParameterIn *newParam, bool head=false)
 
void addParameter (flxParameterIn &newParam, bool head=false)
 
void removeParameter (flxParameterIn *rmParam)
 
void removeParameter (flxParameterIn &rmParam)
 
size_t nInputParameters ()
 
void addParameter (flxParameterOut *newParam, bool head=false)
 
void addParameter (flxParameterOut &newParam, bool head=false)
 
void removeParameter (flxParameterOut *rmParam)
 
void removeParameter (flxParameterOut &rmParam)
 
size_t nOutputParameters ()
 
flxParameterOutList & getOutputParameters (void)
 
flxParameterInList & getInputParameters (void)
 
virtual uint32_t get_epoch (void)=0
 
virtual void set_epoch (const uint32_t &)=0
 
virtual bool valid_epoch (void)=0
 

Static Public Member Functions

static bool isConnected (flxBusI2C &i2cDriver, uint8_t address)
 
static flxDeviceConfidence_t connectedConfidence (void)
 
static const char * getDeviceName ()
 
static const uint8_t * getDefaultAddresses ()
 
- Static Public Member Functions inherited from flxDeviceI2CType< flxDevGNSS >
static flxTypeID type (void)
 
static flxDeviceKind_t kind (void)
 
- Static Public Member Functions inherited from flxObject
static flxTypeID type (void)
 

Public Attributes

flxPropertyRWUInt32< flxDevGNSS, &flxDevGNSS::get_measurement_rate, &flxDevGNSS::set_measurement_rate > measurementRate
 
flxPropertyRWBool< flxDevGNSS, &flxDevGNSS::get_pps_logging, &flxDevGNSS::set_pps_logging > ppsLogging
 
flxPropertyRWUInt16< flxDevGNSS, &flxDevGNSS::get_pps_pin, &flxDevGNSS::set_pps_pin > ppsPin
 
flxParameterInVoid< flxDevGNSS, &flxDevGNSS::factory_default > factoryDefault
 
flxParameterOutUInt32< flxDevGNSS, &flxDevGNSS::read_year > year
 
flxParameterOutUInt32< flxDevGNSS, &flxDevGNSS::read_month > month
 
flxParameterOutUInt32< flxDevGNSS, &flxDevGNSS::read_day > day
 
flxParameterOutUInt32< flxDevGNSS, &flxDevGNSS::read_hour > hour
 
flxParameterOutUInt32< flxDevGNSS, &flxDevGNSS::read_min > min
 
flxParameterOutUInt32< flxDevGNSS, &flxDevGNSS::read_sec > sec
 
flxParameterOutDouble< flxDevGNSS, &flxDevGNSS::read_latitude > latitude
 
flxParameterOutDouble< flxDevGNSS, &flxDevGNSS::read_longitude > longitude
 
flxParameterOutDouble< flxDevGNSS, &flxDevGNSS::read_altitude > altitude
 
flxParameterOutDouble< flxDevGNSS, &flxDevGNSS::read_altitude_msl > altitudeMSL
 
flxParameterOutUInt32< flxDevGNSS, &flxDevGNSS::read_siv > SIV
 
flxParameterOutUInt32< flxDevGNSS, &flxDevGNSS::read_fix > fixType
 
flxParameterOutUInt32< flxDevGNSS, &flxDevGNSS::read_carrier_soln > carrierSolution
 
flxParameterOutFloat< flxDevGNSS, &flxDevGNSS::read_ground_speed > groundSpeed
 
flxParameterOutFloat< flxDevGNSS, &flxDevGNSS::read_heading > heading
 
flxParameterOutFloat< flxDevGNSS, &flxDevGNSS::read_pdop > PDOP
 
flxParameterOutFloat< flxDevGNSS, &flxDevGNSS::read_horiz_acc > horizontalAccEst
 
flxParameterOutFloat< flxDevGNSS, &flxDevGNSS::read_vert_acc > verticalAccEst
 
flxParameterOutUInt32< flxDevGNSS, &flxDevGNSS::read_tow > TOW
 
flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_iso8601 > iso8601
 
flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_yyyy_mm_dd > YYYYMMDD
 
flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_yyyy_dd_mm > YYYYDDMM
 
flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_dd_mm_yyyy > DDMMYYYY
 
flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_hh_mm_ss > HHMMSS
 
flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_fix_string > fixTypeStr
 
flxParameterOutString< flxDevGNSS, &flxDevGNSS::read_carrier_soln_string > carrierSolutionStr
 
flxParameterOutArrayFloat< flxDevGNSS, &flxDevGNSS::get_location > location
 
- Public Attributes inherited from flxDevice
flxParameterInVoid< flxDevice, &flxDevice::disable_all_parameters > disableAllParameters
 
flxParameterInVoid< flxDevice, &flxDevice::enable_all_parameters > enableAllParameters
 

Static Public Attributes

static uint8_t defaultDeviceAddress [] = {kGNSSAddressDefault, kSparkDeviceAddressNull}
 

Additional Inherited Members

- Protected Attributes inherited from flxDescriptor
const char * _name
 
bool _nameAlloc
 
const char * _desc
 
bool _descAlloc
 
const char * _title
 
bool _titleAlloc
 

Constructor & Destructor Documentation

◆ flxDevGNSS()

flxDevGNSS::flxDevGNSS ( )

Member Function Documentation

◆ connectedConfidence()

static flxDeviceConfidence_t flxDevGNSS::connectedConfidence ( void  )
inlinestatic

◆ get_epoch()

uint32_t flxDevGNSS::get_epoch ( void  )
inlinevirtual

Implements flxIClock.

◆ getDefaultAddresses()

static const uint8_t * flxDevGNSS::getDefaultAddresses ( )
inlinestatic

◆ getDeviceName()

static const char * flxDevGNSS::getDeviceName ( )
inlinestatic

◆ isConnected()

bool flxDevGNSS::isConnected ( flxBusI2C &  i2cDriver,
uint8_t  address 
)
static

◆ onInitialize()

bool flxDevGNSS::onInitialize ( TwoWire &  wirePort)
virtual

Reimplemented from flxDeviceI2CType< flxDevGNSS >.

◆ set_epoch()

void flxDevGNSS::set_epoch ( const uint32_t &  refEpoch)
inlinevirtual

Implements flxIClock.

◆ setAvailablePPSPins()

void flxDevGNSS::setAvailablePPSPins ( const uint16_t *  ppsPin,
size_t  len 
)

◆ valid_epoch()

bool flxDevGNSS::valid_epoch ( void  )
inlinevirtual

Implements flxIClock.

Member Data Documentation

◆ altitude

flxParameterOutDouble<flxDevGNSS, &flxDevGNSS::read_altitude> flxDevGNSS::altitude

◆ altitudeMSL

flxParameterOutDouble<flxDevGNSS, &flxDevGNSS::read_altitude_msl> flxDevGNSS::altitudeMSL

◆ carrierSolution

flxParameterOutUInt32<flxDevGNSS, &flxDevGNSS::read_carrier_soln> flxDevGNSS::carrierSolution

◆ carrierSolutionStr

flxParameterOutString<flxDevGNSS, &flxDevGNSS::read_carrier_soln_string> flxDevGNSS::carrierSolutionStr

◆ day

flxParameterOutUInt32<flxDevGNSS, &flxDevGNSS::read_day> flxDevGNSS::day

◆ DDMMYYYY

flxParameterOutString<flxDevGNSS, &flxDevGNSS::read_dd_mm_yyyy> flxDevGNSS::DDMMYYYY

◆ defaultDeviceAddress

uint8_t flxDevGNSS::defaultDeviceAddress = {kGNSSAddressDefault, kSparkDeviceAddressNull}
static

◆ factoryDefault

flxParameterInVoid<flxDevGNSS, &flxDevGNSS::factory_default> flxDevGNSS::factoryDefault

◆ fixType

flxParameterOutUInt32<flxDevGNSS, &flxDevGNSS::read_fix> flxDevGNSS::fixType

◆ fixTypeStr

flxParameterOutString<flxDevGNSS, &flxDevGNSS::read_fix_string> flxDevGNSS::fixTypeStr

◆ groundSpeed

flxParameterOutFloat<flxDevGNSS, &flxDevGNSS::read_ground_speed> flxDevGNSS::groundSpeed

◆ heading

flxParameterOutFloat<flxDevGNSS, &flxDevGNSS::read_heading> flxDevGNSS::heading

◆ HHMMSS

flxParameterOutString<flxDevGNSS, &flxDevGNSS::read_hh_mm_ss> flxDevGNSS::HHMMSS

◆ horizontalAccEst

flxParameterOutFloat<flxDevGNSS, &flxDevGNSS::read_horiz_acc> flxDevGNSS::horizontalAccEst

◆ hour

flxParameterOutUInt32<flxDevGNSS, &flxDevGNSS::read_hour> flxDevGNSS::hour

◆ iso8601

flxParameterOutString<flxDevGNSS, &flxDevGNSS::read_iso8601> flxDevGNSS::iso8601

◆ latitude

flxParameterOutDouble<flxDevGNSS, &flxDevGNSS::read_latitude> flxDevGNSS::latitude

◆ location

flxParameterOutArrayFloat<flxDevGNSS, &flxDevGNSS::get_location> flxDevGNSS::location

◆ longitude

flxParameterOutDouble<flxDevGNSS, &flxDevGNSS::read_longitude> flxDevGNSS::longitude

◆ measurementRate

flxPropertyRWUInt32<flxDevGNSS, &flxDevGNSS::get_measurement_rate, &flxDevGNSS::set_measurement_rate> flxDevGNSS::measurementRate

◆ min

flxParameterOutUInt32<flxDevGNSS, &flxDevGNSS::read_min> flxDevGNSS::min

◆ month

flxParameterOutUInt32<flxDevGNSS, &flxDevGNSS::read_month> flxDevGNSS::month

◆ PDOP

flxParameterOutFloat<flxDevGNSS, &flxDevGNSS::read_pdop> flxDevGNSS::PDOP

◆ ppsLogging

flxPropertyRWBool<flxDevGNSS, &flxDevGNSS::get_pps_logging, &flxDevGNSS::set_pps_logging> flxDevGNSS::ppsLogging

◆ ppsPin

flxPropertyRWUInt16<flxDevGNSS, &flxDevGNSS::get_pps_pin, &flxDevGNSS::set_pps_pin> flxDevGNSS::ppsPin

◆ sec

flxParameterOutUInt32<flxDevGNSS, &flxDevGNSS::read_sec> flxDevGNSS::sec

◆ SIV

flxParameterOutUInt32<flxDevGNSS, &flxDevGNSS::read_siv> flxDevGNSS::SIV

◆ TOW

flxParameterOutUInt32<flxDevGNSS, &flxDevGNSS::read_tow> flxDevGNSS::TOW

◆ verticalAccEst

flxParameterOutFloat<flxDevGNSS, &flxDevGNSS::read_vert_acc> flxDevGNSS::verticalAccEst

◆ year

flxParameterOutUInt32<flxDevGNSS, &flxDevGNSS::read_year> flxDevGNSS::year

◆ YYYYDDMM

flxParameterOutString<flxDevGNSS, &flxDevGNSS::read_yyyy_dd_mm> flxDevGNSS::YYYYDDMM

◆ YYYYMMDD

flxParameterOutString<flxDevGNSS, &flxDevGNSS::read_yyyy_mm_dd> flxDevGNSS::YYYYMMDD

The documentation for this class was generated from the following files: