flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxObject Class Reference

#include <flxCoreProps.h>

Inheritance diagram for flxObject:
flxPersist _flxPropertyContainer flxDescriptor flxOperation flxContainer< flxOperation > flxAction flxDevice flxActionType< _flxClock > flxActionType< flxApplication > flxActionType< flxFSSDCard > flxActionType< flxFSSDMMCard > flxActionType< flxFileRotate > flxActionType< flxIoTArduino > flxActionType< flxLogger > flxActionType< flxOptExtSerial > flxActionType< flxOptInterruptEvent > flxActionType< flxSetWifiCredentials > flxActionType< flxSettingsSave > flxActionType< flxSettingsSerial > flxActionType< flxSysFirmware > flxActionType< flxSystem > flxActionType< flxTimer > flxContainer< flxAction > flxActionType< T > flxContainer< flxDevice > flxDeviceGPIOType< flxDevAnalogPin > flxDeviceGPIOType< flxDevSerial > flxDeviceGPIOType< flxDevSoilMoisture > flxDeviceI2CType< flxDevACS37800 > flxDeviceI2CType< flxDevADS1015 > flxDeviceI2CType< flxDevADS122C04 > flxDeviceI2CType< flxDevAHT20 > flxDeviceI2CType< flxDevAMG8833 > flxDeviceI2CType< flxDevAS7265X > flxDeviceI2CType< flxDevAS7331 > flxDeviceI2CType< flxDevAS7343 > flxDeviceI2CType< flxDevBME280 > flxDeviceI2CType< flxDevBME68x > flxDeviceI2CType< flxDevBMI270 > flxDeviceI2CType< flxDevBMP384 > flxDeviceI2CType< flxDevBMP581 > flxDeviceI2CType< flxDevBMV080 > flxDeviceI2CType< flxDevBioHub > flxDeviceI2CType< flxDevButton > flxDeviceI2CType< flxDevCCS811 > flxDeviceI2CType< flxDevENS160 > flxDeviceI2CType< flxDevFS3000 > flxDeviceI2CType< flxDevGNSS > flxDeviceI2CType< flxDevLPS25HB > flxDeviceI2CType< flxDevMAX17048 > flxDeviceI2CType< flxDevMCP9600 > flxDeviceI2CType< flxDevMS5637 > flxDeviceI2CType< flxDevMS8607 > flxDeviceI2CType< flxDevMicroPressure > flxDeviceI2CType< flxDevNAU7802 > flxDeviceI2CType< flxDevOPT4048 > flxDeviceI2CType< flxDevPASCO2V01 > flxDeviceI2CType< flxDevRV8803 > flxDeviceI2CType< flxDevSCD30 > flxDeviceI2CType< flxDevSCD40 > flxDeviceI2CType< flxDevSDP3X > flxDeviceI2CType< flxDevSEN54 > flxDeviceI2CType< flxDevSGP30 > flxDeviceI2CType< flxDevSGP40 > flxDeviceI2CType< flxDevSHTC3 > flxDeviceI2CType< flxDevST25DV > flxDeviceI2CType< flxDevSTC31 > flxDeviceI2CType< flxDevSTHS34PF80 > flxDeviceI2CType< flxDevTMF882X > flxDeviceI2CType< flxDevTMP117 > flxDeviceI2CType< flxDevTwist > flxDeviceI2CType< flxDevVCNL4040 > flxDeviceI2CType< flxDevVEML6075 > flxDeviceI2CType< flxDevVEML7700 > flxDeviceI2CType< flxDevVL53L1X > flxDeviceI2CType< flxDevVL53L5 > flxDevISM330Base flxDevMMC5983Base flxDeviceGPIOType< T > flxDeviceI2CType< T, B > flxDeviceSPIType< T, B >

Public Member Functions

 flxObject ()
 
virtual ~flxObject ()
 
virtual size_t n_children (void)
 
void setParent (flxObject *parent)
 
void setParent (flxObject &parent)
 
flxObject * parent ()
 
void setHidden (bool bHide=true)
 
bool hidden ()
 
void setIsDirty (bool bDirty=true)
 
bool isDirty (void)
 
virtual bool onSave (flxStorageBlock *stBlk)
 
virtual bool save (flxStorage *pStorage)
 
virtual void restoreComplete (void)
 
virtual bool onRestore (flxStorageBlock *stBlk)
 
virtual bool restore (flxStorage *pStorage)
 
virtual flxTypeID getType (void)
 
virtual bool save (flxStorage *)=0
 
virtual bool restore (flxStorage *)=0
 
- Public Member Functions inherited from _flxPropertyContainer
 _flxPropertyContainer ()
 
void addProperty (flxProperty *newProperty)
 
void addProperty (flxProperty &newProperty)
 
void removeProperty (flxProperty *rmProp)
 
bool containsProperty (flxProperty *prop)
 
void removeProperty (flxProperty &rmProp)
 
flxPropertyList & getProperties (void)
 
uint nProperties (void)
 
bool saveProperties (flxStorageBlock *stBlk)
 
bool restoreProperties (flxStorageBlock *stBlk)
 
size_t propertySaveSize ()
 
void hideProperty (flxProperty &theProp)
 
- Public Member Functions inherited from flxDescriptor
 flxDescriptor ()
 
void setName (const char *new_name)
 Set the Name object - storing the pointer to the provided string No allocation is performed. If the previous name was allocated, it is freed. More...
 
void setName (const char *new_name, const char *new_desc)
 Set the Name object and the Description for the object. Both strings are constants. More...
 
void setName (char *new_name)
 Set the Name object, but makes a copy of the input string since the input is not const. If the previous name was allocated, it is freed. More...
 
const char * name ()
 Return a const char pointer to the name of the object. More...
 
std::string name_ (void)
 Returns a std::string of the name of the object. More...
 
void setDescription (const char *new_desc)
 Set the Description object - the input value is constant and not copied. If the previous description was allocated, it is freed. More...
 
void setDescription (char *new_desc)
 Set the Description object - the input value is not constant and is copied. If the previous description was allocated, it is freed. More...
 
const char * description ()
 Return the constant C string pointer to the description of the object. More...
 
std::string description_ (void)
 Return the description of the object as a std::string. More...
 
void setTitle (const char *title)
 Set the Title object - the title is optional and is used mostly for UX or organizational purposes. The input value is constant and not copied. If the previous title was allocated, it is freed. More...
 
void setTitleAlloc (char *new_title)
 Set the Title of the object , but make an explict copy of the provided string. More...
 
const char * title (void)
 Return the C constant string pointer to the title of the object. More...
 

Static Public Member Functions

static flxTypeID type (void)
 

Additional Inherited Members

- Protected Attributes inherited from flxDescriptor
const char * _name
 
bool _nameAlloc
 
const char * _desc
 
bool _descAlloc
 
const char * _title
 
bool _titleAlloc
 

Constructor & Destructor Documentation

◆ flxObject()

flxObject::flxObject ( )
inline

◆ ~flxObject()

virtual flxObject::~flxObject ( )
inlinevirtual

Member Function Documentation

◆ getType()

virtual flxTypeID flxObject::getType ( void  )
inlinevirtual

Reimplemented in flxOperation, flxActionType< T >, flxActionType< _flxClock >, flxActionType< flxApplication >, flxActionType< flxFSSDCard >, flxActionType< flxFSSDMMCard >, flxActionType< flxFileRotate >, flxActionType< flxIoTArduino >, flxActionType< flxLogger >, flxActionType< flxOptExtSerial >, flxActionType< flxOptInterruptEvent >, flxActionType< flxSetWifiCredentials >, flxActionType< flxSettingsSave >, flxActionType< flxSettingsSerial >, flxActionType< flxSysFirmware >, flxActionType< flxSystem >, flxActionType< flxTimer >, flxContainer< flxAction >, flxContainer< flxDevice >, flxContainer< flxOperation >, flxDeviceI2CType< T, B >, flxDeviceI2CType< flxDevACS37800 >, flxDeviceI2CType< flxDevADS1015 >, flxDeviceI2CType< flxDevADS122C04 >, flxDeviceI2CType< flxDevAHT20 >, flxDeviceI2CType< flxDevAMG8833 >, flxDeviceI2CType< flxDevAS7265X >, flxDeviceI2CType< flxDevAS7331 >, flxDeviceI2CType< flxDevAS7343 >, flxDeviceI2CType< flxDevBME280 >, flxDeviceI2CType< flxDevBME68x >, flxDeviceI2CType< flxDevBMI270 >, flxDeviceI2CType< flxDevBMP384 >, flxDeviceI2CType< flxDevBMP581 >, flxDeviceI2CType< flxDevBMV080 >, flxDeviceI2CType< flxDevBioHub >, flxDeviceI2CType< flxDevButton >, flxDeviceI2CType< flxDevCCS811 >, flxDeviceI2CType< flxDevENS160 >, flxDeviceI2CType< flxDevFS3000 >, flxDeviceI2CType< flxDevGNSS >, flxDeviceI2CType< flxDevISM330, flxDevISM330Base >, flxDeviceI2CType< flxDevLPS25HB >, flxDeviceI2CType< flxDevMAX17048 >, flxDeviceI2CType< flxDevMCP9600 >, flxDeviceI2CType< flxDevMMC5983, flxDevMMC5983Base >, flxDeviceI2CType< flxDevMS5637 >, flxDeviceI2CType< flxDevMS8607 >, flxDeviceI2CType< flxDevMicroPressure >, flxDeviceI2CType< flxDevNAU7802 >, flxDeviceI2CType< flxDevOPT4048 >, flxDeviceI2CType< flxDevPASCO2V01 >, flxDeviceI2CType< flxDevRV8803 >, flxDeviceI2CType< flxDevSCD30 >, flxDeviceI2CType< flxDevSCD40 >, flxDeviceI2CType< flxDevSDP3X >, flxDeviceI2CType< flxDevSEN54 >, flxDeviceI2CType< flxDevSGP30 >, flxDeviceI2CType< flxDevSGP40 >, flxDeviceI2CType< flxDevSHTC3 >, flxDeviceI2CType< flxDevST25DV >, flxDeviceI2CType< flxDevSTC31 >, flxDeviceI2CType< flxDevSTHS34PF80 >, flxDeviceI2CType< flxDevTMF882X >, flxDeviceI2CType< flxDevTMP117 >, flxDeviceI2CType< flxDevTwist >, flxDeviceI2CType< flxDevVCNL4040 >, flxDeviceI2CType< flxDevVEML6075 >, flxDeviceI2CType< flxDevVEML7700 >, flxDeviceI2CType< flxDevVL53L1X >, flxDeviceI2CType< flxDevVL53L5 >, flxDeviceSPIType< T, B >, flxDeviceSPIType< flxDevISM330_SPI, flxDevISM330Base >, flxDeviceSPIType< flxDevMMC5983_SPI, flxDevMMC5983Base >, flxDeviceGPIOType< T >, flxDeviceGPIOType< flxDevAnalogPin >, flxDeviceGPIOType< flxDevSerial >, and flxDeviceGPIOType< flxDevSoilMoisture >.

◆ hidden()

bool flxObject::hidden ( )
inline

◆ isDirty()

bool flxObject::isDirty ( void  )
inline

◆ n_children()

virtual size_t flxObject::n_children ( void  )
inlinevirtual

◆ onRestore()

virtual bool flxObject::onRestore ( flxStorageBlock *  stBlk)
inlinevirtual

Reimplemented in flxOperation.

◆ onSave()

virtual bool flxObject::onSave ( flxStorageBlock *  stBlk)
inlinevirtual

Reimplemented in flxOperation.

◆ parent()

flxObject * flxObject::parent ( )
inline

◆ restore()

virtual bool flxObject::restore ( flxStorage *  pStorage)
inlinevirtual

◆ restoreComplete()

virtual void flxObject::restoreComplete ( void  )
inlinevirtual

Reimplemented in flxDevBMV080.

◆ save()

virtual bool flxObject::save ( flxStorage *  pStorage)
inlinevirtual

◆ setHidden()

void flxObject::setHidden ( bool  bHide = true)
inline

◆ setIsDirty()

void flxObject::setIsDirty ( bool  bDirty = true)
inline

◆ setParent() [1/2]

void flxObject::setParent ( flxObject &  parent)
inline

◆ setParent() [2/2]

void flxObject::setParent ( flxObject *  parent)
inline

◆ type()

static flxTypeID flxObject::type ( void  )
inlinestatic

The documentation for this class was generated from the following file: