flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxLoggingDrvDefault Class Reference

#include <flxCoreLog.h>

Inheritance diagram for flxLoggingDrvDefault:
flxLoggingDriver

Public Member Functions

 flxLoggingDrvDefault ()
 
int logPrintf (const flxLogLevel_t level, bool newline, const char *fmt, va_list args)
 
void setOutput (flxWriter &theWriter)
 
void setOutput (flxWriter *theWriter)
 
- Public Member Functions inherited from flxLoggingDriver
virtual int logPrintf (const flxLogLevel_t level, bool newline, const char *fmt, va_list args)=0
 
virtual void setLogLevel (flxLogLevel_t level)
 

Constructor & Destructor Documentation

◆ flxLoggingDrvDefault()

flxLoggingDrvDefault::flxLoggingDrvDefault ( )
inline

Member Function Documentation

◆ logPrintf()

int flxLoggingDrvDefault::logPrintf ( const flxLogLevel_t  level,
bool  newline,
const char *  fmt,
va_list  args 
)
virtual

Implements flxLoggingDriver.

◆ setOutput() [1/2]

void flxLoggingDrvDefault::setOutput ( flxWriter &  theWriter)
inline

◆ setOutput() [2/2]

void flxLoggingDrvDefault::setOutput ( flxWriter *  theWriter)
inline

The documentation for this class was generated from the following files: