flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
_flxPropertyTyped< Object, T, HIDDEN, SECURE > Class Template Reference

#include <flxCoreProps.h>

Inheritance diagram for _flxPropertyTyped< Object, T, HIDDEN, SECURE >:
_flxPropertyBase< T, HIDDEN, SECURE > flxProperty _flxDataIn< T > _flxDataOut< T > flxDescriptor flxDataIn flxDataOut

Public Member Functions

 _flxPropertyTyped ()
 
 _flxPropertyTyped (T value)
 
 _flxPropertyTyped (T min, T max)
 
 _flxPropertyTyped (T value, T min, T max)
 
 _flxPropertyTyped (std::initializer_list< std::pair< const std::string, T > > limitSet)
 
 _flxPropertyTyped (T value, std::initializer_list< std::pair< const std::string, T > > limitSet)
 
void operator() (Object *me)
 
void operator() (Object *obj, const char *name)
 
void operator() (Object *obj, const char *name, const char *desc)
 
T get () const
 Get the value of the object as a templated type. A pure virtual method. More...
 
void set (T const &value)
 
bool operator> (int rhs)
 
bool operator== (const T &rhs)
 
T operator() () const
 
void operator() (T const &value)
 
 operator T () const
 
_flxPropertyTyped< Object, T, HIDDEN, SECURE > & operator= (T const &value)
 
- Public Member Functions inherited from _flxPropertyBase< T, HIDDEN, SECURE >
 _flxPropertyBase ()
 
bool hidden ()
 
void setHidden (void)
 
bool secure ()
 
flxDataType_t type ()
 
virtual size_t size ()
 
virtual size_t save_size ()
 
virtual T get (void) const =0
 Get the value of the object as a templated type. A pure virtual method. More...
 
virtual void set (T const &value)=0
 
bool save (flxStorageBlock *stBlk)
 
bool restore (flxStorageBlock *stBlk)
 
virtual std::string to_string (void)
 
flxEditResult_t editValue (flxDataEditor &theEditor)
 
bool setValue (flxDataVariable &value)
 
flxDataVariable getValue (void)
 
flxDataLimit * dataLimit (void)
 
virtual flxDataType_t type (void)=0
 
virtual flxEditResult_t editValue (flxDataEditor &)=0
 
virtual flxDataLimit * dataLimit (void)=0
 
virtual bool setValue (flxDataVariable &)=0
 
virtual flxDataVariable getValue (void)=0
 
virtual bool hidden (void)=0
 
virtual void setHidden (void)=0
 
virtual bool secure (void)=0
 
virtual size_t size (void)
 
virtual size_t save_size (void)
 
virtual std::string to_string ()
 
virtual bool save (flxStorageBlock *)=0
 
virtual bool restore (flxStorageBlock *)=0
 
- Public Member Functions inherited from flxDescriptor
 flxDescriptor ()
 
void setName (const char *new_name)
 Set the Name object - storing the pointer to the provided string No allocation is performed. If the previous name was allocated, it is freed. More...
 
void setName (const char *new_name, const char *new_desc)
 Set the Name object and the Description for the object. Both strings are constants. More...
 
void setName (char *new_name)
 Set the Name object, but makes a copy of the input string since the input is not const. If the previous name was allocated, it is freed. More...
 
const char * name ()
 Return a const char pointer to the name of the object. More...
 
std::string name_ (void)
 Returns a std::string of the name of the object. More...
 
void setDescription (const char *new_desc)
 Set the Description object - the input value is constant and not copied. If the previous description was allocated, it is freed. More...
 
void setDescription (char *new_desc)
 Set the Description object - the input value is not constant and is copied. If the previous description was allocated, it is freed. More...
 
const char * description ()
 Return the constant C string pointer to the description of the object. More...
 
std::string description_ (void)
 Return the description of the object as a std::string. More...
 
void setTitle (const char *title)
 Set the Title object - the title is optional and is used mostly for UX or organizational purposes. The input value is constant and not copied. If the previous title was allocated, it is freed. More...
 
void setTitleAlloc (char *new_title)
 Set the Title of the object , but make an explict copy of the provided string. More...
 
const char * title (void)
 Return the C constant string pointer to the title of the object. More...
 
- Public Member Functions inherited from _flxDataIn< T >
 _flxDataIn ()
 
flxDataType_t type (void)
 
virtual void set (T const &value)=0
 
void setBool (bool value)
 
void setInt8 (int8_t value)
 
void setInt16 (int16_t value)
 
void setInt32 (int32_t value)
 
void setUInt8 (uint8_t value)
 
void setUInt16 (uint16_t value)
 
void setUInt32 (uint32_t value)
 
void setFloat (float value)
 
void setDouble (double value)
 
void setString (std::string &value)
 
void setDataLimit (flxDataLimitType< T > &dataLimit)
 
void setDataLimit (flxDataLimitType< T > *dataLimit)
 
flxDataLimit * dataLimit (void)
 
void setDataLimitRange (T min, T max)
 
void setDataLimitRange (std::pair< T, T > range)
 
void addDataLimitValidValue (std::string name, T value)
 
void addDataLimitValidValue (std::pair< const std::string, T > value)
 
void addDataLimitValidValue (std::initializer_list< std::pair< const std::string, T > > limitSet)
 
void clearDataLimit (void)
 
bool isValueValid (T value)
 
- Public Member Functions inherited from flxDataIn
virtual flxDataType_t type (void)=0
 
virtual void setBool (bool)=0
 
virtual void setInt8 (int8_t)=0
 
virtual void setInt16 (int16_t)=0
 
virtual void setInt32 (int32_t)=0
 
virtual void setUInt8 (uint8_t)=0
 
virtual void setUInt16 (uint16_t)=0
 
virtual void setUInt32 (uint32_t)=0
 
virtual void setFloat (float)=0
 
virtual void setDouble (double)=0
 
virtual void setString (std::string &)=0
 
void set_value (bool v)
 
void set_value (int8_t v)
 
void set_value (int16_t v)
 
void set_value (int32_t v)
 
void set_value (uint8_t v)
 
void set_value (uint16_t v)
 
void set_value (uint32_t v)
 
void set_value (float v)
 
void set_value (double v)
 
void set_value (std::string &v)
 
- Public Member Functions inherited from _flxDataOut< T >
flxDataType_t type (void)
 Returns the data type of the object - based on the templated type. More...
 
virtual T get (void) const =0
 Get the value of the object as a templated type. A pure virtual method. More...
 
bool getBool ()
 Get the Bool value of the object. More...
 
int8_t getInt8 ()
 Get the int8 value of the object. More...
 
int16_t getInt16 ()
 Get the int16 value of the object. More...
 
int32_t getInt32 ()
 Get the int32 value of the object. More...
 
uint8_t getUInt8 ()
 Get the uint8 value of the object. More...
 
uint16_t getUInt16 ()
 Get the uint16 value of the object. More...
 
uint32_t getUInt32 ()
 Get the uint32 value of the object. More...
 
float getFloat ()
 Get the float value of the object. More...
 
double getDouble ()
 Get the double value of the object. More...
 
std::string getString ()
 Get the string value of the object. More...
 
- Public Member Functions inherited from flxDataOut
virtual flxDataType_t type (void)=0
 Return the type of the data. More...
 
virtual bool getBool ()=0
 Get the data as a boolean. More...
 
virtual int8_t getInt8 ()=0
 Get the data as an int8_t. More...
 
virtual int16_t getInt16 ()=0
 Get the data as an int16_t. More...
 
virtual int32_t getInt32 ()=0
 Get the data as an int32_t. More...
 
virtual uint8_t getUInt8 ()=0
 Get the data as a uint8_t. More...
 
virtual uint16_t getUInt16 ()=0
 Get the data as a uint16_t. More...
 
virtual uint32_t getUInt32 ()=0
 Get the data as a uint32_t. More...
 
virtual float getFloat ()=0
 Get the data as a float. More...
 
virtual double getDouble ()=0
 Get the data as a double. More...
 
virtual std::string getString ()=0
 Get the data as a string. More...
 
bool get_value (bool b)
 Get the value object as a bool. More...
 
int8_t get_value (int8_t)
 Get the value object as an int8_t. More...
 
int16_t get_value (int16_t)
 Get the value object as an int16_t. More...
 
int32_t get_value (int32_t)
 Get the value object as an int32_t. More...
 
uint8_t get_value (uint8_t)
 Get the value object as a uint8_t. More...
 
uint16_t get_value (uint16_t)
 Get the value object as a uint16_t. More...
 
uint32_t get_value (uint32_t)
 Get the value object as a uint32_t. More...
 
float get_value (float)
 Get the value object as a float. More...
 
double get_value (double)
 Get the value object as a double. More...
 
std::string get_value (std::string)
 Get the value object as a string. More...
 

Additional Inherited Members

- Public Types inherited from _flxDataOut< T >
typedef T value_type
 A public member that is of the type of this object. Handy for templated code. More...
 
- Protected Attributes inherited from flxDescriptor
const char * _name
 
bool _nameAlloc
 
const char * _desc
 
bool _descAlloc
 
const char * _title
 
bool _titleAlloc
 

Constructor & Destructor Documentation

◆ _flxPropertyTyped() [1/6]

template<class Object , class T , bool HIDDEN = false, bool SECURE = false>
_flxPropertyTyped< Object, T, HIDDEN, SECURE >::_flxPropertyTyped ( )
inline

◆ _flxPropertyTyped() [2/6]

template<class Object , class T , bool HIDDEN = false, bool SECURE = false>
_flxPropertyTyped< Object, T, HIDDEN, SECURE >::_flxPropertyTyped ( T  value)
inline

◆ _flxPropertyTyped() [3/6]

template<class Object , class T , bool HIDDEN = false, bool SECURE = false>
_flxPropertyTyped< Object, T, HIDDEN, SECURE >::_flxPropertyTyped ( T  min,
T  max 
)
inline

◆ _flxPropertyTyped() [4/6]

template<class Object , class T , bool HIDDEN = false, bool SECURE = false>
_flxPropertyTyped< Object, T, HIDDEN, SECURE >::_flxPropertyTyped ( T  value,
T  min,
T  max 
)
inline

◆ _flxPropertyTyped() [5/6]

template<class Object , class T , bool HIDDEN = false, bool SECURE = false>
_flxPropertyTyped< Object, T, HIDDEN, SECURE >::_flxPropertyTyped ( std::initializer_list< std::pair< const std::string, T > >  limitSet)
inline

◆ _flxPropertyTyped() [6/6]

template<class Object , class T , bool HIDDEN = false, bool SECURE = false>
_flxPropertyTyped< Object, T, HIDDEN, SECURE >::_flxPropertyTyped ( T  value,
std::initializer_list< std::pair< const std::string, T > >  limitSet 
)
inline

Member Function Documentation

◆ get()

template<class Object , class T , bool HIDDEN = false, bool SECURE = false>
T _flxPropertyTyped< Object, T, HIDDEN, SECURE >::get ( ) const
inlinevirtual

Get the value of the object as a templated type. A pure virtual method.

Returns
T

Implements _flxPropertyBase< T, HIDDEN, SECURE >.

◆ operator T()

template<class Object , class T , bool HIDDEN = false, bool SECURE = false>
_flxPropertyTyped< Object, T, HIDDEN, SECURE >::operator T ( ) const
inline

◆ operator()() [1/5]

template<class Object , class T , bool HIDDEN = false, bool SECURE = false>
T _flxPropertyTyped< Object, T, HIDDEN, SECURE >::operator() ( ) const
inline

◆ operator()() [2/5]

template<class Object , class T , bool HIDDEN = false, bool SECURE = false>
void _flxPropertyTyped< Object, T, HIDDEN, SECURE >::operator() ( Object *  me)
inline

◆ operator()() [3/5]

template<class Object , class T , bool HIDDEN = false, bool SECURE = false>
void _flxPropertyTyped< Object, T, HIDDEN, SECURE >::operator() ( Object *  obj,
const char *  name 
)
inline

◆ operator()() [4/5]

template<class Object , class T , bool HIDDEN = false, bool SECURE = false>
void _flxPropertyTyped< Object, T, HIDDEN, SECURE >::operator() ( Object *  obj,
const char *  name,
const char *  desc 
)
inline

◆ operator()() [5/5]

template<class Object , class T , bool HIDDEN = false, bool SECURE = false>
void _flxPropertyTyped< Object, T, HIDDEN, SECURE >::operator() ( T const &  value)
inline

◆ operator=()

template<class Object , class T , bool HIDDEN = false, bool SECURE = false>
_flxPropertyTyped< Object, T, HIDDEN, SECURE > & _flxPropertyTyped< Object, T, HIDDEN, SECURE >::operator= ( T const &  value)
inline

◆ operator==()

template<class Object , class T , bool HIDDEN = false, bool SECURE = false>
bool _flxPropertyTyped< Object, T, HIDDEN, SECURE >::operator== ( const T &  rhs)
inline

◆ operator>()

template<class Object , class T , bool HIDDEN = false, bool SECURE = false>
bool _flxPropertyTyped< Object, T, HIDDEN, SECURE >::operator> ( int  rhs)
inline

◆ set()

template<class Object , class T , bool HIDDEN = false, bool SECURE = false>
void _flxPropertyTyped< Object, T, HIDDEN, SECURE >::set ( T const &  value)
inlinevirtual

The documentation for this class was generated from the following file: