📄️ MicroSD Card Setup
Not all microSD cards are created equal. The capacity, read/write speed, and format vary depending on the manufacturer. In order to log data to the microSD card, you will need to ensure that your memory card is formatted as FAT32. You can also use FAT16. If the memory card is formatted as a different memory card, the DataLogger IoT will not be able to recognize the microSD card.
📄️ Serial Terminals
The key to the setup and interactive operation of the the SparkFun DataLoggerIoT is a modern, interactive Serial Terminal program. Keyboard input and text output are required to be immdiate, to support the interactive menu system of the IoT DataLoggerIoT. Luckily a majority of serial terminal support interactive use. The notible exeception is the build in Arduino IDE Serial Monitor, which requires text to be entered and "submitted" or sent to the device. The Arduino Serial Monitor is not supported for interactive use by the DataLoggerIoT
📄️ Downloads
DataLogger IoT - 9DoF
📄️ Supported Devices
The following lists the devices/boards supported by the DataLogger IoT boards. New drivers to support a device will be listed under the firmware version.
📄️ Release Notes
SparkFun DataLogger IoT Firmware - Version 1.5
📄️ Suggested Reading
* If you aren't familiar with the Qwiic system, we recommend reading here for an overview.