📄️ Logger Setup
In the Settings menu, select the Logger menu to adjust how data is logged, including what additional data to provide besides sensor readings.
📄️ Logging Timer
In the Settings menu, select the Timer option adjust the Logging Timer period value.
📄️ Logging - Data File
A key feature of the DataLoggerIoT is logging data to an IoT web service, but it still performs core data logging functionality, including logging data to a file on an SD card.
📄️ Interrupt Trigger
This option is used to setup an external interrupt as a trigger for a logging event. By connecting an external device that will trigger an interrupt to a GPIO pin on the DataLoggerIoT, an external device can cause an log event to occur.