📄️ External Serial
This menu item is used to configure logging from an external serial device that is connected to the datalogger via GPIO pins.
📄️ Soil Mosture Sensor
The DataLoggerIoT can support reading values from a GPIO connected, resistive Soil Moisture sensor, like the SparkFun Soil Moisture Sensor. When connected to the datalogger, and enabled, the DataLoggerIoT will read the analog moisture value from the sensor and add that to the output log stream.
📄️ Analog Pin Sensor
This menu item is used to enable the GPIO Analog Pin Device within the DataLoggerIoT. When enabled, an Analog Pin Reading device driver is added to the dataloggers Device Settings list.