Skip to main content

Analog Pin Sensor

This menu item is used to enable the GPIO Analog Pin Device within the DataLoggerIoT. When enabled, an Analog Pin Reading device driver is added to the dataloggers Device Settings list.

Enabling the Analog Pin Sensor​

Once the analog device is connected to a supported gpio analog pin on the datalogger, the Analog Pin device is enabled using the Analog Pin Sensor menu item located under the GPIO Devices header. This is enabled using the following menu item:

GPIO Analog Pin Sensor

Once enabled, a Analog Pin Reading device is added to the DataLogger IoT.

Analog Pin Device

Analog Pin Reading Device​

The Analog Pin Reading device has the following menu:

Analog Pin Settings

Settings​

Enable this sensor​

Used to enable the device

Sensor Pin​

The datalogger GPIO pin to read the analog value from. This is the pin the external analog device is connected to.

Value values for this are:

  • A0
  • A3
  • A7

Analog Pin Values