Skip to main content

External Serial

This menu item is used to configure logging from an external serial device that is connected to the datalogger via GPIO pins.

Selecting this option brings up the following menu:

External Serial Menu

Settings​

Serial Settings​

These settings define the parameters of the connected device.

RX Pin​

The GPIO pin on the DataLoggerIoT to use as the RX pin for communicating with the external device. The default pin is 16.

TX Pin​

The GPIO pin on the DataLoggerIoT to use as the TX pin for communicating with the external device. The default pin is 17.

Baud Rate​

Set this to the Baud Rate to use when communicating with the external device.

Functionality​

Serial Input Device​

When enabled, the system create a "Serial Input Device" that is added as a device to the system. This device is used to read data from the external device via a Serial connection and is used just like any other device in the system.

Serial Device

Serial Device​

When the serial device is enabled, a "Serial Device" driver is added to the Device List of the DataLoggerIoT.

Selecting this device from the Device Settings page of the menu system, brings up the following menu:

Serial Device Menu

The device is fairly simple - you enable/disable it and when a log event occurs, any value available in the serial device is read as a string and output to the log stream.

Additionally, when this device is enabled, when data is available from the serial device, a log event is triggered so that the data is read. This is done to prevent the underlying serial device buffer from overflowing.

Settings​

Enable​

Used to enable the device. When enabled, when data is available on the Serial device, it triggers a log event, which will read and log the data in the device.