Skip to main content

Interrupt Trigger

This option is used to setup an external interrupt as a trigger for a logging event. By connecting an external device that will trigger an interrupt to a GPIO pin on the DataLoggerIoT, an external device can cause an log event to occur.

When this menu item is selected, the following settings menu is displayed:

Logging Interrupt Menu

Logger Interrupt Menu Options

Settings​

The settings for this feature are the following:

Enabled​

Use this setting to enable/disable this functionality

Event Name​

A string that represents the "name" of the logging event. This name can be displayed using the "event source" option of the Logger.

Interrupt Pin​

The DataLoggerIoT GPIO Pin to use to detect the external interrupt. Valid pins are: 33 and 36 and selected in the options menu.