Skip to main content

Logger Setup

In the Settings menu, select the Logger menu to adjust how data is logged, including what additional data to provide besides sensor readings.

When this menu option is selected, the following menu is presented:

Logger Menu Options

Logger Menu Options

Details of menu item are outlined in the following sections.

Settings​

Timestamp Mode​

This setting is used to add a timestamp to the output logging stream for each data sample/observation. The format of the timestamp is also selected.

The options for this settings are:

  • No Timestamp - no timestamp is added to the output - this is the default option
  • Milliseconds since program start - Time since the system was started, in milliseconds
  • Seconds since Epoch - Seconds since epoch (January 1, 1970 00:00:00.00 UTC). A valid system time is required for this value to be accurate.
  • Milliseconds since Epoch - Milliseconds since epoch (January 1, 1970 00:00:00.00 UTC). A valid system time is required for this value to be accurate.
  • Date Time - USA Date format - a data/time string formatted using standard US date format - MM-DD-YYYY
  • Date Time - A standard non-USA formatted date string - DD-MM-YYYY
  • ISO8601 Timestamp - an ISO8601 formatted timestamp
  • ISO8601 Timestamp with Time Zone - an ISO8601 formatted timestamp with the current time zone included
  • ISO8601 Timestamp - Week Date - an ISO8601 formatted timestamp using a week date format
  • ISO8601 Timestamp - Week Date with Time Zone - an ISO8601 formatted timestamp using a week date format and the current time zone.

Sample Numbering​

The "sample number" for a the logged data is included in the log stream. This is incremented with each log event by the value of the Number Increment setting value

Numbering Increment​

The amount to increment the output Sample Number after each logged observation.

Output ID​

Include the DataLoggerIoT board ID in the output log stream

Output Name​

Include the DataLoggerIoT board Name in the output log stream

Rate Metric​

If enabled, the system will record the logging data rate. This is helpful in determining the performance of the datalogger.

Output Source Name​

When enabled, the source of the logging event is included in the log stream. This could include values like 'timer', 'GPIO Interrupt', 'GNSS PPS' ...etc.

Output​

These settings are used to control output format and additional values for the datalogger.

SD Card Format​

The format used when writing to the SD Card - options are CSV, JSON, or None.

Serial Console Format​

The format used when writing data to the serial console - options are CSV, JSON, or None.

System Info​

When enabled, the following data is added to the log stream:

  • WiFi SSID
  • WiFi RSSI
  • System uptime
  • System SD Card free space
  • System memory heap

Functions​

Reset Sample Counter​

This will reset the sample counter in the logger to a provided value.

Example Output​

The following image is JSON formatted serial console output for the datalogger. The following options are enabled:

  • Timestamp enabled - ISO8601 Timestamp format
  • Board ID
  • Board Name
  • Trigger source
  • System Info

DataLogger IoT Re-Initializing and Outputting Time in ISO08601 Time Format

JSON Formatted Log Output to the Serial Console