Skip to main content

NTP Client Setup

NTP - Network Time Protocol - It is a networking protocol used to synchronize the clocks of computers over a network. NTP ensures that all devices on a network maintain the same accurate time, which is crucial for various applications such as logging events, security protocols, and time-sensitive transactions.

When connected to the network (via WiFi), the DataLoggerIoT can use NTP as a time refernce. To do this, NTP must be enabled and NTP services to use specified. The configuration of NTP for the DataLoggerIoT is enabled in this secton of the Settings menu.

NTP Configuration​

In the Settings menu, under the Network heading, select the NTP Client settings.

NTP Client Menu Options

NTP Client

The NTP configuration has the following settings:

SettingDescription
EnabledUsed to Enable or Disable the use of NTP by the DataLoggerIoT
NTP Server OneThe primary NTP Server to use. Default value is: pool.ntp.org*
NTP Server TwoThe secondary NTP Server to use. Default value is: time.nist.gov
note

Only one NTP service is required to use this option, but it's common to provice two for redundancy.

Once changes are made to the NTP settings, the should take effect immediatly.