flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
_flxClock Class Reference

#include <flxClock.h>

Inheritance diagram for _flxClock:
flxActionType< _flxClock > flxAction flxOperation flxObject _flxParameterContainer flxPersist _flxPropertyContainer flxDescriptor

Public Member Functions

 _flxClock (_flxClock const &)=delete
 
void operator= (_flxClock const &)=delete
 
uint32_t epoch ()
 
uint32_t now ()
 
void setSystemClock (flxISystemClock *clock)
 
bool setReferenceClock (flxIClock *clock, const char *name=nullptr)
 
void addReferenceClock (flxIClock *clock, const char *name=nullptr)
 
int addConnectedClock (flxIClock *clock)
 
void updateClock (void)
 
void updateConnectedClocks (void)
 
bool initialize (void)
 
- Public Member Functions inherited from flxActionType< _flxClock >
flxTypeID getType (void)
 
virtual bool initialize (void)
 
- Public Member Functions inherited from flxOperation
virtual flxTypeID getType (void)
 
virtual bool execute (void)
 Virtual method called to run the operation - called before data is retrieved. More...
 
virtual bool onSave (flxStorageBlock *stBlk)
 
virtual bool onRestore (flxStorageBlock *stBlk)
 
- Public Member Functions inherited from flxObject
 flxObject ()
 
virtual ~flxObject ()
 
virtual size_t n_children (void)
 
void setParent (flxObject *parent)
 
void setParent (flxObject &parent)
 
flxObject * parent ()
 
void setHidden (bool bHide=true)
 
bool hidden ()
 
void setIsDirty (bool bDirty=true)
 
bool isDirty (void)
 
virtual bool onSave (flxStorageBlock *stBlk)
 
virtual bool save (flxStorage *pStorage)
 
virtual void restoreComplete (void)
 
virtual bool onRestore (flxStorageBlock *stBlk)
 
virtual bool restore (flxStorage *pStorage)
 
virtual flxTypeID getType (void)
 
virtual bool save (flxStorage *)=0
 
virtual bool restore (flxStorage *)=0
 
- Public Member Functions inherited from _flxPropertyContainer
 _flxPropertyContainer ()
 
void addProperty (flxProperty *newProperty)
 
void addProperty (flxProperty &newProperty)
 
void removeProperty (flxProperty *rmProp)
 
bool containsProperty (flxProperty *prop)
 
void removeProperty (flxProperty &rmProp)
 
flxPropertyList & getProperties (void)
 
uint nProperties (void)
 
bool saveProperties (flxStorageBlock *stBlk)
 
bool restoreProperties (flxStorageBlock *stBlk)
 
size_t propertySaveSize ()
 
void hideProperty (flxProperty &theProp)
 
- Public Member Functions inherited from flxDescriptor
 flxDescriptor ()
 
void setName (const char *new_name)
 Set the Name object - storing the pointer to the provided string No allocation is performed. If the previous name was allocated, it is freed. More...
 
void setName (const char *new_name, const char *new_desc)
 Set the Name object and the Description for the object. Both strings are constants. More...
 
void setName (char *new_name)
 Set the Name object, but makes a copy of the input string since the input is not const. If the previous name was allocated, it is freed. More...
 
const char * name ()
 Return a const char pointer to the name of the object. More...
 
std::string name_ (void)
 Returns a std::string of the name of the object. More...
 
void setDescription (const char *new_desc)
 Set the Description object - the input value is constant and not copied. If the previous description was allocated, it is freed. More...
 
void setDescription (char *new_desc)
 Set the Description object - the input value is not constant and is copied. If the previous description was allocated, it is freed. More...
 
const char * description ()
 Return the constant C string pointer to the description of the object. More...
 
std::string description_ (void)
 Return the description of the object as a std::string. More...
 
void setTitle (const char *title)
 Set the Title object - the title is optional and is used mostly for UX or organizational purposes. The input value is constant and not copied. If the previous title was allocated, it is freed. More...
 
void setTitleAlloc (char *new_title)
 Set the Title of the object , but make an explict copy of the provided string. More...
 
const char * title (void)
 Return the C constant string pointer to the title of the object. More...
 
- Public Member Functions inherited from _flxParameterContainer
void addParameter (flxParameterIn *newParam, bool head=false)
 
void addParameter (flxParameterIn &newParam, bool head=false)
 
void removeParameter (flxParameterIn *rmParam)
 
void removeParameter (flxParameterIn &rmParam)
 
size_t nInputParameters ()
 
void addParameter (flxParameterOut *newParam, bool head=false)
 
void addParameter (flxParameterOut &newParam, bool head=false)
 
void removeParameter (flxParameterOut *rmParam)
 
void removeParameter (flxParameterOut &rmParam)
 
size_t nOutputParameters ()
 
flxParameterOutList & getOutputParameters (void)
 
flxParameterInList & getInputParameters (void)
 

Static Public Member Functions

static _flxClock & get (void)
 
- Static Public Member Functions inherited from flxActionType< _flxClock >
static flxTypeID type (void)
 
- Static Public Member Functions inherited from flxObject
static flxTypeID type (void)
 

Public Attributes

flxPropertyRWString< _flxClock, &_flxClock::get_ref_clock, &_flxClock::set_ref_clock > referenceClock
 
flxPropertyRWUInt32< _flxClock, &_flxClock::get_ref_interval, &_flxClock::set_ref_interval > updateClockInterval
 
flxPropertyBool< _flxClock > useAlternativeClock = {true}
 
flxPropertyRWUInt32< _flxClock, &_flxClock::get_conn_interval, &_flxClock::set_conn_interval > connectedClockInterval = {60}
 
flxPropertyBool< _flxClock > updateConnectedOnUpdate = {true}
 
flxPropertyRWString< _flxClock, &_flxClock::get_timezone, &_flxClock::set_timezone > timeZone
 

Additional Inherited Members

- Protected Attributes inherited from flxDescriptor
const char * _name
 
bool _nameAlloc
 
const char * _desc
 
bool _descAlloc
 
const char * _title
 
bool _titleAlloc
 

Constructor & Destructor Documentation

◆ _flxClock()

_flxClock::_flxClock ( _flxClock const &  )
delete

Member Function Documentation

◆ addConnectedClock()

int _flxClock::addConnectedClock ( flxIClock *  clock)

◆ addReferenceClock()

void _flxClock::addReferenceClock ( flxIClock *  clock,
const char *  name = nullptr 
)

◆ epoch()

uint32_t _flxClock::epoch ( )

◆ get()

static _flxClock & _flxClock::get ( void  )
inlinestatic

◆ initialize()

bool _flxClock::initialize ( void  )
virtual

Reimplemented from flxAction.

◆ now()

uint32_t _flxClock::now ( )

◆ operator=()

void _flxClock::operator= ( _flxClock const &  )
delete

◆ setReferenceClock()

bool _flxClock::setReferenceClock ( flxIClock *  clock,
const char *  name = nullptr 
)

◆ setSystemClock()

void _flxClock::setSystemClock ( flxISystemClock *  clock)

◆ updateClock()

void _flxClock::updateClock ( void  )

◆ updateConnectedClocks()

void _flxClock::updateConnectedClocks ( void  )

Member Data Documentation

◆ connectedClockInterval

flxPropertyRWUInt32<_flxClock, &_flxClock::get_conn_interval, &_flxClock::set_conn_interval> _flxClock::connectedClockInterval = {60}

◆ referenceClock

flxPropertyRWString<_flxClock, &_flxClock::get_ref_clock, &_flxClock::set_ref_clock> _flxClock::referenceClock

◆ timeZone

flxPropertyRWString<_flxClock, &_flxClock::get_timezone, &_flxClock::set_timezone> _flxClock::timeZone
Initial value:
= {
#define kClockTimeZoneSparkFun
Definition: flxClock.h:21

◆ updateClockInterval

flxPropertyRWUInt32<_flxClock, &_flxClock::get_ref_interval, &_flxClock::set_ref_interval> _flxClock::updateClockInterval
Initial value:
= {
60}

◆ updateConnectedOnUpdate

flxPropertyBool<_flxClock> _flxClock::updateConnectedOnUpdate = {true}

◆ useAlternativeClock

flxPropertyBool<_flxClock> _flxClock::useAlternativeClock = {true}

The documentation for this class was generated from the following files: