flux sdk  v01.05.00-6-g190c94c
Embedded C++ SDK
Loading...
Searching...
No Matches
flxLogger Class Reference

#include <flxLogger.h>

Inheritance diagram for flxLogger:
flxActionType< flxLogger > flxAction flxOperation flxObject _flxParameterContainer flxPersist _flxPropertyContainer flxDescriptor

Public Types

enum  Timestamp_t {
  TimeStampNone , TimeStampMillis , TimeStampEpoch , TimeStampEpochMillis ,
  TimeStampDateTimeUSA , TimeStampDateTime , TimeStampISO8601 , TimeStampISO8601TZ ,
  TimeStampISO8601WD , TimeStampISO8601WDTZ
}
 

Public Member Functions

 flxLogger ()
 
void logMessage (char *header, char *message)
 
template<typename... Args>
 flxLogger (flxOutputFormat *a1, Args &&...args)
 
template<typename... Args>
 flxLogger (flxOutputFormat &a1, Args &&...args)
 
template<typename... Args>
 flxLogger (flxOperation *a1, Args &...args)
 
template<typename... Args>
 flxLogger (flxOperation &a1, Args &...args)
 
template<typename... Args>
 flxLogger (flxParameterOut *a1, Args &...args)
 
template<typename... Args>
 flxLogger (flxParameterOut &a1, Args &...args)
 
void logObservation (void)
 
void logObservationWithSource (const char *source)
 
void listen (flxSignalVoid &theEvent)
 
void listen (flxSignalString &theEvent)
 
template<typename T >
void logObservation (T value)
 
template<typename T >
void listen (T &theEvent)
 
void logEvent (flxOperation *theObj)
 
void listenLogEvent (flxSignalVoid &theEvent, flxOperation *theObj)
 
template<typename T >
void logEvent (flxOperation *theObj, T value)
 
template<typename T >
void listenLogEvent (T &theEvent, flxOperation *theObj)
 
template<typename... Args>
void add (flxOutputFormat *a1, Args &&...args)
 
template<typename... Args>
void add (flxOutputFormat &a1, Args &&...args)
 
template<typename... Args>
void add (flxOperation &a1, Args &&...args)
 
template<typename... Args>
void add (flxOperation *a1, Args &&...args)
 
template<typename... Args>
void add (flxParameterOut *a1, Args &&...args)
 
template<typename... Args>
void add (flxParameterOut &a1, Args &&...args)
 
template<typename... Args>
void add (flxParameterOutList &a1, Args &&...args)
 
template<typename... Args>
void add (flxProperty &a1, Args &&...args)
 
template<typename... Args>
void add (flxProperty *a1, Args &&...args)
 
template<typename... Args>
void add (flxPropertyList &a1, Args &&...args)
 
template<typename... Args>
void remove (flxOperation &a1, Args &&...args)
 
template<typename... Args>
void remove (flxOperation *a1, Args &&...args)
 
void setEnableLogRate (bool enable)
 
bool enabledLogRate (void)
 
float getLogRate (void)
 
- Public Member Functions inherited from flxActionType< flxLogger >
flxTypeID getType (void)
 
- Public Member Functions inherited from flxAction
virtual bool initialize (void)
 
- Public Member Functions inherited from flxOperation
virtual flxTypeID getType (void)
 
virtual bool execute (void)
 Virtual method called to run the operation - called before data is retrieved. More...
 
virtual bool onSave (flxStorageBlock *stBlk)
 
virtual bool onRestore (flxStorageBlock *stBlk)
 
- Public Member Functions inherited from flxObject
 flxObject ()
 
virtual ~flxObject ()
 
virtual size_t n_children (void)
 
void setParent (flxObject *parent)
 
void setParent (flxObject &parent)
 
flxObject * parent ()
 
void setHidden (bool bHide=true)
 
bool hidden ()
 
void setIsDirty (bool bDirty=true)
 
bool isDirty (void)
 
virtual bool onSave (flxStorageBlock *stBlk)
 
virtual bool save (flxStorage *pStorage)
 
virtual void restoreComplete (void)
 
virtual bool onRestore (flxStorageBlock *stBlk)
 
virtual bool restore (flxStorage *pStorage)
 
virtual flxTypeID getType (void)
 
virtual bool save (flxStorage *)=0
 
virtual bool restore (flxStorage *)=0
 
- Public Member Functions inherited from _flxPropertyContainer
 _flxPropertyContainer ()
 
void addProperty (flxProperty *newProperty)
 
void addProperty (flxProperty &newProperty)
 
void removeProperty (flxProperty *rmProp)
 
bool containsProperty (flxProperty *prop)
 
void removeProperty (flxProperty &rmProp)
 
flxPropertyList & getProperties (void)
 
uint nProperties (void)
 
bool saveProperties (flxStorageBlock *stBlk)
 
bool restoreProperties (flxStorageBlock *stBlk)
 
size_t propertySaveSize ()
 
void hideProperty (flxProperty &theProp)
 
- Public Member Functions inherited from flxDescriptor
 flxDescriptor ()
 
void setName (const char *new_name)
 Set the Name object - storing the pointer to the provided string No allocation is performed. If the previous name was allocated, it is freed. More...
 
void setName (const char *new_name, const char *new_desc)
 Set the Name object and the Description for the object. Both strings are constants. More...
 
void setName (char *new_name)
 Set the Name object, but makes a copy of the input string since the input is not const. If the previous name was allocated, it is freed. More...
 
const char * name ()
 Return a const char pointer to the name of the object. More...
 
std::string name_ (void)
 Returns a std::string of the name of the object. More...
 
void setDescription (const char *new_desc)
 Set the Description object - the input value is constant and not copied. If the previous description was allocated, it is freed. More...
 
void setDescription (char *new_desc)
 Set the Description object - the input value is not constant and is copied. If the previous description was allocated, it is freed. More...
 
const char * description ()
 Return the constant C string pointer to the description of the object. More...
 
std::string description_ (void)
 Return the description of the object as a std::string. More...
 
void setTitle (const char *title)
 Set the Title object - the title is optional and is used mostly for UX or organizational purposes. The input value is constant and not copied. If the previous title was allocated, it is freed. More...
 
void setTitleAlloc (char *new_title)
 Set the Title of the object , but make an explict copy of the provided string. More...
 
const char * title (void)
 Return the C constant string pointer to the title of the object. More...
 
- Public Member Functions inherited from _flxParameterContainer
void addParameter (flxParameterIn *newParam, bool head=false)
 
void addParameter (flxParameterIn &newParam, bool head=false)
 
void removeParameter (flxParameterIn *rmParam)
 
void removeParameter (flxParameterIn &rmParam)
 
size_t nInputParameters ()
 
void addParameter (flxParameterOut *newParam, bool head=false)
 
void addParameter (flxParameterOut &newParam, bool head=false)
 
void removeParameter (flxParameterOut *rmParam)
 
void removeParameter (flxParameterOut &rmParam)
 
size_t nOutputParameters ()
 
flxParameterOutList & getOutputParameters (void)
 
flxParameterInList & getInputParameters (void)
 

Public Attributes

flxPropertyRWUInt32< flxLogger, &flxLogger::get_ts_type, &flxLogger::set_ts_type > timestampMode
 
flxParameterOutString< flxLogger, &flxLogger::get_timestamp > timestamp
 
flxPropertyRWBool< flxLogger, &flxLogger::get_id_enable, &flxLogger::set_id_enable > enableIDOutput = {false}
 
flxParameterOutString< flxLogger, &flxLogger::get_device_id > getDeviceID
 
flxPropertyRWBool< flxLogger, &flxLogger::get_name_enable, &flxLogger::set_name_enable > enableNameOutput = {false}
 
flxParameterOutString< flxLogger, &flxLogger::get_name > getLocalName
 
flxPropertyRWBool< flxLogger, &flxLogger::get_num_mode, &flxLogger::set_num_mode > numberMode = {false}
 
flxParameterOutUInt32< flxLogger, &flxLogger::get_sample_number > sampleNumber
 
flxPropertyUInt32< flxLogger > numberIncrement = {1, 1, 10000}
 
flxParameterInUInt32< flxLogger, &flxLogger::reset_sample_number > resetSampleNumber = {0, 10000}
 
flxPropertyRWBool< flxLogger, &flxLogger::enabledLogRate, &flxLogger::setEnableLogRate > logRateMetric = {false}
 
flxPropertyRWBool< flxLogger, &flxLogger::get_source_enable, &flxLogger::set_source_enable > enableSourceNameOutput
 
flxParameterOutString< flxLogger, &flxLogger::get_source > logEventSourceName
 

Additional Inherited Members

- Static Public Member Functions inherited from flxActionType< flxLogger >
static flxTypeID type (void)
 
- Static Public Member Functions inherited from flxObject
static flxTypeID type (void)
 
- Protected Attributes inherited from flxDescriptor
const char * _name
 
bool _nameAlloc
 
const char * _desc
 
bool _descAlloc
 
const char * _title
 
bool _titleAlloc
 

Member Enumeration Documentation

◆ Timestamp_t

Enumerator
TimeStampNone 
TimeStampMillis 
TimeStampEpoch 
TimeStampEpochMillis 
TimeStampDateTimeUSA 
TimeStampDateTime 
TimeStampISO8601 
TimeStampISO8601TZ 
TimeStampISO8601WD 
TimeStampISO8601WDTZ 

Constructor & Destructor Documentation

◆ flxLogger() [1/7]

flxLogger::flxLogger ( )

◆ flxLogger() [2/7]

template<typename... Args>
flxLogger::flxLogger ( flxOutputFormat *  a1,
Args &&...  args 
)
inline

◆ flxLogger() [3/7]

template<typename... Args>
flxLogger::flxLogger ( flxOutputFormat &  a1,
Args &&...  args 
)
inline

◆ flxLogger() [4/7]

template<typename... Args>
flxLogger::flxLogger ( flxOperation *  a1,
Args &...  args 
)
inline

◆ flxLogger() [5/7]

template<typename... Args>
flxLogger::flxLogger ( flxOperation &  a1,
Args &...  args 
)
inline

◆ flxLogger() [6/7]

template<typename... Args>
flxLogger::flxLogger ( flxParameterOut *  a1,
Args &...  args 
)
inline

◆ flxLogger() [7/7]

template<typename... Args>
flxLogger::flxLogger ( flxParameterOut &  a1,
Args &...  args 
)
inline

Member Function Documentation

◆ add() [1/10]

template<typename... Args>
void flxLogger::add ( flxOperation &  a1,
Args &&...  args 
)
inline

◆ add() [2/10]

template<typename... Args>
void flxLogger::add ( flxOperation *  a1,
Args &&...  args 
)
inline

◆ add() [3/10]

template<typename... Args>
void flxLogger::add ( flxOutputFormat &  a1,
Args &&...  args 
)
inline

◆ add() [4/10]

template<typename... Args>
void flxLogger::add ( flxOutputFormat *  a1,
Args &&...  args 
)
inline

◆ add() [5/10]

template<typename... Args>
void flxLogger::add ( flxParameterOut &  a1,
Args &&...  args 
)
inline

◆ add() [6/10]

template<typename... Args>
void flxLogger::add ( flxParameterOut *  a1,
Args &&...  args 
)
inline

◆ add() [7/10]

template<typename... Args>
void flxLogger::add ( flxParameterOutList &  a1,
Args &&...  args 
)
inline

◆ add() [8/10]

template<typename... Args>
void flxLogger::add ( flxProperty &  a1,
Args &&...  args 
)
inline

◆ add() [9/10]

template<typename... Args>
void flxLogger::add ( flxProperty *  a1,
Args &&...  args 
)
inline

◆ add() [10/10]

template<typename... Args>
void flxLogger::add ( flxPropertyList &  a1,
Args &&...  args 
)
inline

◆ enabledLogRate()

bool flxLogger::enabledLogRate ( void  )
inline

◆ getLogRate()

float flxLogger::getLogRate ( void  )

◆ listen() [1/3]

void flxLogger::listen ( flxSignalString &  theEvent)
inline

◆ listen() [2/3]

void flxLogger::listen ( flxSignalVoid &  theEvent)
inline

◆ listen() [3/3]

template<typename T >
void flxLogger::listen ( T &  theEvent)
inline

◆ listenLogEvent() [1/2]

void flxLogger::listenLogEvent ( flxSignalVoid &  theEvent,
flxOperation *  theObj 
)
inline

◆ listenLogEvent() [2/2]

template<typename T >
void flxLogger::listenLogEvent ( T &  theEvent,
flxOperation *  theObj 
)
inline

◆ logEvent() [1/2]

void flxLogger::logEvent ( flxOperation *  theObj)
inline

◆ logEvent() [2/2]

template<typename T >
void flxLogger::logEvent ( flxOperation *  theObj,
T  value 
)
inline

◆ logMessage()

void flxLogger::logMessage ( char *  header,
char *  message 
)

◆ logObservation() [1/2]

template<typename T >
void flxLogger::logObservation ( T  value)
inline

◆ logObservation() [2/2]

void flxLogger::logObservation ( void  )

◆ logObservationWithSource()

void flxLogger::logObservationWithSource ( const char *  source)

◆ remove() [1/2]

template<typename... Args>
void flxLogger::remove ( flxOperation &  a1,
Args &&...  args 
)
inline

◆ remove() [2/2]

template<typename... Args>
void flxLogger::remove ( flxOperation *  a1,
Args &&...  args 
)
inline

◆ setEnableLogRate()

void flxLogger::setEnableLogRate ( bool  enable)

Member Data Documentation

◆ enableIDOutput

flxPropertyRWBool<flxLogger, &flxLogger::get_id_enable, &flxLogger::set_id_enable> flxLogger::enableIDOutput = {false}

◆ enableNameOutput

flxPropertyRWBool<flxLogger, &flxLogger::get_name_enable, &flxLogger::set_name_enable> flxLogger::enableNameOutput = {false}

◆ enableSourceNameOutput

flxPropertyRWBool<flxLogger, &flxLogger::get_source_enable, &flxLogger::set_source_enable> flxLogger::enableSourceNameOutput
Initial value:
=
{false}

◆ getDeviceID

flxParameterOutString<flxLogger, &flxLogger::get_device_id> flxLogger::getDeviceID

◆ getLocalName

flxParameterOutString<flxLogger, &flxLogger::get_name> flxLogger::getLocalName

◆ logEventSourceName

flxParameterOutString<flxLogger, &flxLogger::get_source> flxLogger::logEventSourceName

◆ logRateMetric

◆ numberIncrement

flxPropertyUInt32<flxLogger> flxLogger::numberIncrement = {1, 1, 10000}

◆ numberMode

flxPropertyRWBool<flxLogger, &flxLogger::get_num_mode, &flxLogger::set_num_mode> flxLogger::numberMode = {false}

◆ resetSampleNumber

flxParameterInUInt32<flxLogger, &flxLogger::reset_sample_number> flxLogger::resetSampleNumber = {0, 10000}

◆ sampleNumber

flxParameterOutUInt32<flxLogger, &flxLogger::get_sample_number> flxLogger::sampleNumber

◆ timestamp

flxParameterOutString<flxLogger, &flxLogger::get_timestamp> flxLogger::timestamp

◆ timestampMode

flxPropertyRWUInt32<flxLogger, &flxLogger::get_ts_type, &flxLogger::set_ts_type> flxLogger::timestampMode
Initial value:
= {
{
{"No Timestamp", TimeStampNone},
{"Milliseconds since program start", TimeStampMillis},
{"Seconds since Epoch", TimeStampEpoch},
{"Milliseconds since Epoch", TimeStampEpochMillis},
{"Date Time - USA Date format", TimeStampDateTimeUSA},
{"Date Time", TimeStampDateTime},
{"ISO8601 Timestamp", TimeStampISO8601},
{"ISO8601 Timestamp with Time Zone", TimeStampISO8601TZ},
{"ISO8601 Timestamp - Week Date", TimeStampISO8601WD},
{"ISO8601 Timestamp - Week Date with Time Zone", TimeStampISO8601WDTZ},
}}
@ TimeStampISO8601
Definition: flxLogger.h:283
@ TimeStampEpochMillis
Definition: flxLogger.h:280
@ TimeStampEpoch
Definition: flxLogger.h:279
@ TimeStampISO8601WD
Definition: flxLogger.h:285
@ TimeStampDateTime
Definition: flxLogger.h:282
@ TimeStampISO8601WDTZ
Definition: flxLogger.h:286
@ TimeStampDateTimeUSA
Definition: flxLogger.h:281
@ TimeStampNone
Definition: flxLogger.h:277
@ TimeStampMillis
Definition: flxLogger.h:278
@ TimeStampISO8601TZ
Definition: flxLogger.h:284

The documentation for this class was generated from the following files: